LPC55s28 Documentation conflict

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55s28 Documentation conflict

1,270 Views
andrewfisher
Contributor III

Please can someone eplain which is the correct information in these 2 directly conflicting documents.

AN13037 : Section 3.2.3 : PIN/DFLT

UM11126 : Table 1064.Access restriction levels

 

See definitions of permanently enabled and permanently disabled

This is really poor as getting these settings wrong can brick your chip!

 

Which is right?

1 Reply

1,262 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello andrewfisher,

The description with AN13037 is right.

Sorry for the inconvenient to you.

 

BR

Alice

 

BR

Alice

0 Kudos
Reply