lpc540xx XIP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc540xx XIP

1,248件の閲覧回数
amakmal
Contributor I

Hi,

Where can i find the code which do XIP (Execution In Place) from external SPI flash (Micron), in the SDK there is Download image XIP example, but I need to run code from the external flash in XIP, 

Thanks In advance

Avi Makmal

WINBOND

0 件の賞賛
返信
1 返信

1,183件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Avi Makmal

Could you please provide more information of which LPC are you using? 

Please take a look into the following application note: 

Which explains how to modify the header structure of the image in order to run code from the external flash. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信