lpc4370 DAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc4370 DAC

1,894 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Mon May 26 22:18:12 MST 2014
Hello friends,


I am using LPC-Link ii board for my project. In the schematic diagram of the board, I saw  EXP_ADC0_DAC pin. I know ADC0 and DAC are connected internally and ADC0 is P4.3 and DAC is P4.4 . However I was wondering if I can use EXP_ADC0_DAC pin for DAC operation or not?

Please help me regarding this.

Labels (1)
0 Kudos
Reply
3 Replies

1,846 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Sun Aug 24 00:46:04 MST 2014
Hi,

I just want to confirm one more time. I tried to use EXP_ADC_DAC of LPC-link2 board for DAC purpose, it doesn't work. You can find part of my code here . Are you sure I can use this pin for DAC? please help me regarding this.

0 Kudos
Reply

1,846 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri May 30 11:51:28 MST 2014
Hi,

Yes the EXP_ADC0_DAC pin can be used for ADC functionality or DAC functionality.

Thanks,
NXP Technical Support
0 Kudos
Reply

1,846 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by adi nata on Fri May 30 05:48:38 MST 2014
Hello

I use lpc4330, that have same pin for adc0 and dac, i can use it as adc or dac
0 Kudos
Reply