lpc4357 dualcore project configuration problems using keil uvision4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc4357 dualcore project configuration problems using keil uvision4

1,013 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nirvana_xun on Wed Sep 25 00:40:00 MST 2013
hi,all. i am new to lpc4357, so getting problems when creating a dualcore project in uvision4. in both mcb4300 and lpcopen demos, there are example projects(simple blinky) show how to configure a dualcore project, it seems that i can either use target memory layout dialog or user scatter file to achieve this, also some source code or the fromelf.exe may needed to create an image, when running, M4 may load the image and boot M0. the problem is that i do not have an overall idea about the configuration and booting procedure, though the demos works fine, i have problems configure my project. any one gives an idea to help me get familiar with all these things? thanks
Labels (1)
0 Kudos
Reply
0 Replies