lpc2368 under reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc2368 under reset

1,269 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc_doctor on Mon Nov 24 10:18:44 MST 2014
hi,
i have lpc2368 board i designed.
i can programming lpc2368 via isp and jtag(ulink). so everthing is ok. but after programming lpc stops to working. i think it is in state of reset. how can i check it is runnnig or not.

thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,202 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Sun Dec 21 17:15:23 MST 2014
Hi,

You can program a simple blinky program to check an LED or toggle a pin. There are many example for LPC23xx which you can use.

http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-%CE...

Thanks,
NXP Technical Support
0 Kudos
Reply