lpc1817 jtag disabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpc1817 jtag disabled

1,896 次查看
josvisser
Contributor II

I have a few boards with an LPC1817 on which the JTAG is no longer working.

I have checked all the conditions that may disable the JTAG.

- Pin 28 DBGEN is not connected and pulled up internally

- OTP bank 3 is not progammed

- The CRP is not active

- CREG5 is not loaded

Can anybody give me a hint why the JTAG stops working.

I have connected both LPC-Link2 and J-LinkPro without success.

I can only program through ISP.

Regards,

Jos

标签 (1)
0 项奖励
回复
2 回复数

1,745 次查看
bernhardfink
NXP Employee
NXP Employee

Hi Jos,

sometimes SWD ist still working when JTAG is not.So make a crosscheck.

Reason could be a damage of one of the JTAG inputs. See this thread for more details:

https://community.nxp.com/thread/487475 

Regards,

Bernhard.

1,745 次查看
josvisser
Contributor II

Thanks Bernhard,

We will have a closer look at the connection sequence and grounding of power and jtag at our production facility.

Regards,

Jos

0 项奖励
回复