lpc1788 clock/oscillator stops

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1788 clock/oscillator stops

846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nagarajan on Wed May 13 00:11:56 MST 2015
lpc1788 clock/ oscillator stops above +60 DegC or +40degC with humidity of >90% RH and recovers back as the temperature falls below +55 DegC. the device is rated to operate in the range of -40 DegC to 85 DegC.
What could be the cause? can sombody reply?
Advice solution pls. 
ラベル(1)
0 件の賞賛
返信
0 返答(返信)