lpc1788 SD card connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc1788 SD card connection

1,501 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Imagineme on Tue Dec 04 03:30:41 MST 2012
I have the following question i`ve seen development  boards based on lpc1788 and all of them use SPI to access SD card when the MCU has sd card controller.I read that using four-bit SD bus is somehow closed licence and in order to use it i have to pay for i, my question is is that so and if yes can i use 1-bit SD bus for free(and where i can find code examples) or this  SD card controller is off limits (so to speak) for hobby electronics.
Labels (1)
0 Kudos
Reply
1 Reply

1,193 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Tue Dec 04 13:51:09 MST 2012
SD card on LPC1788 is working fine.

You may use this software which contains a working block driver:
http://www.lpcware.com/content/forum/lpc1788-mci-problems#comment-1866

Search a free FAT fs library, and you are almost done..

The SD card organisation does not enforce to sign a licence agreement for private use.
0 Kudos
Reply