lpc1768 programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1768 programming

2,600件の閲覧回数
ali7117117111
Contributor I

I have an lpc1768 processor. I want to program it using (ST link v2 or universal programmer) but I cannot. Can I program it or what is the circuit?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,584件の閲覧回数
frank_m
Senior Contributor III

I tried that some years ago, and it worked well to some degree.I did not do extensive tests, though.
You would need a toolchain/IDE that supports both the LPC MCU and the ST-Link debugger.

Segger has a firmware for the (onboard) ST-Link, to convert it into a JLink.
That would work as well, but Segger's licence conditions explicitly prohibit the use for any other target than STM32s.

But Segger has a similiar firmware for LPC-Links. https://www.segger.com/products/debug-probes/j-link/models/other-j-links/lpc-link-2/
Perhaps worth a try, if you have one.

0 件の賞賛
返信

2,591件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ali7117117111 

LPC1768 doesn't support ST debugger.

Do you have other debuggers, J-link? MCU-link from NXP? Or P&E Universal Multilink ? 

Or any other LPC NXP demo board? Mostly there is debugger on demo board. You can use it.

 

BR

Alice

0 件の賞賛
返信