lpc1768 i2s dma

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1768 i2s dma

1,803件の閲覧回数
sankalp_agrawal
Contributor I

So, I'm trying to interface LPC1768 with PCM5102. I have the I2S module ready and SD card module. The wave file from SD. Now my question how do I sync everything up? Like, DMA will read from SD and directly put it onto the I2S buffer? That's what I think will happen. I haven't tried it out yet but is that the right way to go?

Thanks

ラベル(3)
0 件の賞賛
返信
1 返信

1,664件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sankalp,

Regarding your question that the PCM data are saved in a file on SD card, you want to read the PCM data from the file and play the PCM via the codec PCM5102.

I suppose that the LPC1768 is a bit old, I suggest you use the LPC54xxx or the other processor, which has I2S, SD card interface, EMC intertface with which you can connect SDAM, SRAM, Timer,...

We have developed the SD card example, which supports creating directory/ file system, open file, read/write data to File. I suppose you can use the file system, open file, read PCM to internal SRAM or external SDRAM. Configure the I2S module, and DMA, the DMA can read data from RAM(either SDRAM or internal RAM) to I2S transmitter data register.

This is the LPC54xxx link:

LPC54000|Power Efficient 32-bit Microcontrollers (MCUs)|Cortex®-M4 Core | NXP 

We have developed the SDK package, which includes the SD card driver, I2S driver, I2S example based on interrupt and DMA.

MCUXpresso SDK | NXP 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信