lpc1768 adc power down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc1768 adc power down

Jump to solution
4,278 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by unknownobj on Mon Jun 06 02:03:06 MST 2016
hi, all

i am working on lpc1768 adc now, and the code to do the polling of adc works.
and then i want to use the power down of adc to minimize  the current,
so i set the PDN bit(ADC_PowerDownCmd)  before the adc function and clear it after adc.
i fount that the ADC_ChannelGetStatus function returns zero after ADC_StartCmd.

why?  how can i let adc go to power down mode and repower it before adc function?

any help is appreciated.
Labels (1)
0 Kudos
Reply
1 Solution
3,893 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Customer,

 

     Before you clear PDN to 0, please also clear LPC_AD0CR[START]=000.

   This is very important.

pastedImage_1.png

Please check this point, and try again.


Have a great day,

Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

6 Replies
3,894 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Customer,

 

     Before you clear PDN to 0, please also clear LPC_AD0CR[START]=000.

   This is very important.

pastedImage_1.png

Please check this point, and try again.


Have a great day,

Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,893 Views
billbrown
Contributor I

Thank you so much Kerry,

That fixed the problem.  

I would press the correct answer button if I could find one.

Best regards

Bill

0 Kudos
Reply
3,893 Views
billbrown
Contributor I

I have a similar problem using a LPC-4078.  The ADC runs fine until I go into, and then come out of power down mode.

To maximize power saving, I shut off the PDN bit in the CR register prior to turning off the clocks as the users manual suggests.  But when I wake up and reverse that process, (turn on clocks in PCONP register and then turn on PDN bit in CR register) I no longer get conversion complete on the ADC.  

Any thoughts?

0 Kudos
Reply
3,893 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bill,

     The same as LPC1769,  please check ADC control register START bit, please set it to no start(0x0) when you clearing PDN to 0.

27.jpg

  Please try it on your side.

If you still have question, please contact me!

Please check this point, and try again.

 

 


Have a great day,

Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,893 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply
3,893 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by unknownobj on Sun Jun 12 18:09:51 MST 2016
anyone help
0 Kudos
Reply