lpc1768 adc power down problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc1768 adc power down problem

1,040 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by unknownobj on Sun Jun 12 18:21:59 MST 2016
hi, all

i am working on lpc1768 adc now, and the code to do the polling of adc works.
and then i want to use the power down of adc to minimize the current,
so i set the PDN bit(ADC_PowerDownCmd) before the adc function and clear it after adc.
i fount that the ADC_ChannelGetStatus function returns zero after ADC_StartCmd.

why? how can i let adc go to power down mode and repower it up before adc sampling?

any help is appreciated.
Labels (1)
0 Kudos
Reply
1 Reply

963 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply