lpc1766 cmsis driver library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1766 cmsis driver library

1,659件の閲覧回数
tongjunju
Contributor I

Where can I download the lpc1766 cmsis driver library?

ラベル(2)
0 件の賞賛
返信
1 返信

1,479件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

You can download the driver library from the following link:

CMSISprojects - ** Code Red Support Site ** 

However the use of LPCOpen is now recommended for most LPC MCUs, rather than the 'old-style' CMSIS-CORE library projects and examples. For more details please see the LPCXpresso IDE/MCUXpresso User Manual, and visit the LPCOpen webpages.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信