lpc1549 eagle files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1549 eagle files

6,154件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by opprud on Wed Jul 23 01:20:58 MST 2014
Hi,

i am searching for an eagle library containing the lpc1549 - LQFP48. Can anyone help, or point a direction :-)

best regards
Opprud
ラベル(1)
0 件の賞賛
返信
7 返答(返信)

5,948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cgroen on Thu Aug 14 00:37:20 MST 2014

Quote: DAMEK
hey,

look at this tool / blogpost LPCXpert

it's a ms access db where you can configure your device and export it. as part of it, it creates eagle lib files and altalium files.

greatings



Ahh, thanks a lot :)
0 件の賞賛
返信

5,948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DAMEK on Thu Aug 14 00:01:54 MST 2014
hey,

look at this tool / blogpost LPCXpert

it's a ms access db where you can configure your device and export it. as part of it, it creates eagle lib files and altalium files.

greatings
0 件の賞賛
返信

5,948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cgroen on Sat Aug 09 08:33:13 MST 2014
I'm also looking for a eagle PCB symbol for the 1549 (both 48 and 100 pin), anyone ?
0 件の賞賛
返信

5,948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Jul 25 09:32:04 MST 2014
Hi All,
If you need  orCAD and Allegro footprints,we have those at

http://www.lpcware.com/content/nxpfile/lpc1500-orcad-footprint
http://www.lpcware.com/content/nxpfile/lpc1500-allegro-footprints

and orCAD schematic symbol at

http://www.lpcware.com/content/nxpfile/lpc1500-orcad-schematic-symbol.

Right now we do not have eagle files
0 件の賞賛
返信

5,945件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Thu Jul 24 02:39:14 MST 2014
That's also a good opportunity to rethink pin function/usage of the board.

Especially ISP / Bootloader (CAN/UART/USB) and analog pins...

So drawing your own symbol is helping a lot to avoid surprises later...

I've added my favorite symbol with my usual pin functions  :bigsmile:

0 件の賞賛
返信

5,945件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by opprud on Thu Jul 24 01:41:55 MST 2014
thanks, ill find a somewhat matching lpc13xx-48 part and do that ;-)
0 件の賞賛
返信

5,945件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Jul 23 02:05:50 MST 2014
There's no Eagle library available, but a standard LQFP48 isn't too difficult...

Just download something like:

lpc1xxx-v6.lbr

from

http://www.cadsoft.de/downloads/libraries

and copy/change a LPC13xx LQFP48 for your needs...
0 件の賞賛
返信