lpc11u68 uart clrc663

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc11u68 uart clrc663

1,228 Views
Roll
Contributor I

Hi everyone.  I should have to read the UID value from a RFID reader (with CLRC663) chip using uart interface, with a LPC11u68jbd100 microcontroller. I now have the c language driver code for nxp of the spi interface and the serial port script driver code. Now we want the c language library for the serial port and example code. Thank you in advance for your attention and for what you'll do for me. Good work. Nice day.

0 Kudos
Reply
1 Reply

1,206 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Roll,

It appears that you requires the source code or library for the UART for LPC11U68, if it is the case, pls download the LPCopen package from the link, in includes the package based IAR, Keil and LPCXpresso tools.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply