lpc11e68 SPI effective rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc11e68 SPI effective rate

1,632 Views
eranrai
Contributor I

Hi,

I'm using LPC11e68 system clock is set to 48MHz and SSP0 configured as SPI master @ 12MHz.

it seems like effective baud rate is much lower - DMA is not in used and from the analysis i made it seems like reads/writes to SSP0 DR registers stalls.

did anyone experience any similar performance issues with SPI?

i will appreciate any input.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,521 Views
chrispflieger
Contributor IV

If your SPI is set to 1/4 the CPU speed, you've only got 32 cycles for each byte. That's not much time for the CPU to do too much.

0 Kudos
Reply