lpc11c24 on-chip drivers exception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc11c24 on-chip drivers exception

1,164 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nickich on Mon Jul 06 07:05:35 MST 2015
Hello,

I'm getting HardFault exception when the fourth CAN message appear on the bus.
The stack:
Thread #1 <main> (Suspended : Signal : SIGSTOP:Stopped (signal))
HardFault_Handler() at cr_startup_lpc11xx.c:706 0xd6
<signal handler called>() at 0xfffffff1
0x887766
0x1fff2c1e

It looks it's something inside the ROM drivers. Is there any way to debug this?
What could cause it?

First 3 CAN messages are received OK. When the 4th message appears on the bus the LPC throws this exception. Even the CAN ISR (CAN_rx() ) doesn't get called.

Regards,
Labels (1)
0 Kudos
Reply
1 Reply

1,145 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nickich on Mon Jul 06 07:34:58 MST 2015
...the RAM allocated for the ROM drivers... ;-)
0 Kudos
Reply