lpc1115 FatFS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc1115 FatFS

1,153 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by urb4nm on Mon Aug 19 03:07:21 MST 2013
Hi,
Has anyone tried using FatFS with lpc1115? I can't get it to work. i think it's either a problem with initializing SPI, or, more likely, with mmc.c file, which is an interface between uC and library files... I've been messing with for quite some time, so my code might be a mess, but still, maybe someone has done it..

SPI INIT
void init_spi(void)
{
LPC_IOCON->SCK_LOC=0x01;
LPC_IOCON->PIO0_8=0x01;
LPC_IOCON->PIO0_9=0x01;
LPC_IOCON->PIO2_11=0x01;

LPC_GPIO2->DIR = (1<<8);
LPC_GPIO2->MASKED_ACCESS[(1<<8)] = ~0; //CS HIGH

 
LPC_SSP0->CR0 = (7 << SSPCR0_DSS);// SPI, 8bitów, tryb 0
LPC_SSP0->CPSR = 12;          //Preskaler
LPC_SSP0->CR1 = SSPCR1_SSE;//Uruchomienie SSP0
}


MMC.C
/*------------------------------------------------------------------------*/
/* LPCXpresso176x: MMCv3/SDv1/SDv2 (SPI mode) control module              */
/*------------------------------------------------------------------------*/
/*
/  Copyright (C) 2011, ChaN, all right reserved.
/
/ * This software is a free software and there is NO WARRANTY.
/ * No restriction on use. You can use, modify and redistribute it for
/   personal, non-profit or commercial products UNDER YOUR RESPONSIBILITY.
/ * Redistributions of source code must retain the above copyright notice.
/
/-------------------------------------------------------------------------*/
#include "LPC11xx.h"
#include "diskio.h"
#include "sspAdr.h"
#include "spi.h"

#define SSP_CH0/* SSP channel to use (0:SSP0, 1:SSP1) */

#defineCCLK100000000UL/* cclk frequency [Hz] */
#define PCLK_SSP50000000UL/* PCLK frequency for SSP [Hz] */
#define SCLK_FAST25000000UL/* SCLK frequency under normal operation [Hz] */
#defineSCLK_SLOW400000UL/* SCLK frequency under initialization [Hz] */

BYTE INS = 1;

//#defineINS(!(FIO2PIN1 & _BV(1)))/* Socket status (true:Inserted, false:Empty) */
#defineWP0 /* Card write protection (true:yes, false:no) */
#define CS (1<<8)

#if SSP_CH == 0
#defineSSPxDRSSP_SSP0DR
#defineSSPxSRSSP_SSP0SR
#defineSSPxCR0SSP_SSP0CR0
#defineSSPxCR1SSP_SSP0CR1
#defineSSPxCPSRSSP_SSP0CPSR
#defineCS_LOW(){LPC_GPIO2->MASKED_ACCESS[CS] = ~0;}
#defineCS_HIGH(){LPC_GPIO2->MASKED_ACCESS[CS] = 0;}
//#define PCSSPxPCSSP0
//#definePCLKSSPxPCLK_SSP0
#elif SSP_CH == 1
#defineSSPxDRSSP_SSP1DR
#defineSSPxSRSSP_SSP1SR
#defineSSPxCR0SSP_SSP1CR0
#defineSSPxCR1SSP_SSP1CR1
#defineSSPxCPSRSSP_SSP1CPSR
#defineCS_LOW(){LPC_GPIO2->MASKED_ACCESS[CS] = ~0;}
#defineCS_HIGH(){LPC_GPIO2->MASKED_ACCESS[CS] = 0;}
//#define PCSSPxPCSSP1
//#definePCLKSSPxPCLK_SSP1
#endif

#if PCLK_SSP * 1 == CCLK
#define PCLKDIV_SSPPCLKDIV_1
#elif PCLK_SSP * 2 == CCLK
#define PCLKDIV_SSPPCLKDIV_2
#elif PCLK_SSP * 4 == CCLK
#define PCLKDIV_SSPPCLKDIV_4
#elif PCLK_SSP * 8 == CCLK
#define PCLKDIV_SSPPCLKDIV_8
#else
#error Invalid clock frequency.
#endif


//#define FCLK_FAST() { SSPxCPSR = (PCLK_SSP / SCLK_FAST) & ~1; }
//#define FCLK_SLOW() { SSPxCPSR = (PCLK_SSP / SCLK_SLOW) & ~1; }
static void FCLK_SLOW()
{
    /* Divide by 5 (SSPCLKDIV also enables to SSP CLK) */
    SCB_SSP1CLKDIV = SCB_SSP1CLKDIV_DIV5;

    /* (PCLK / (CPSDVSR * [SCR+1])) = (7,200,000 / (2 x [8 + 1])) = 400 KHz */
    uint32_t configReg = ( SSP_SSP1CR0_DSS_8BIT   // Data size = 8-bit
                  | SSP_SSP1CR0_FRF_SPI           // Frame format = SPI
                  | SSP_SSP1CR0_SCR_8);           // Serial clock rate = 8

    // Set clock polarity (low between frames)
    // configReg &= ~SSP_SSP1CR0_CPOL_MASK;
    // configReg |= SSP_SSP1CR0_CPOL_LOW;

    // Set edge transition (leading edge)
    // configReg &= ~SSP_SSP1CR0_CPHA_MASK;
    // configReg |= SSP_SSP1CR0_CPHA_FIRST;

    // Assign config values to SSP1CR0
    SSP_SSP1CR0 = configReg;

    /* Clock prescale register must be even and at least 2 in master mode */
    SSP_SSP1CPSR = SSP_SSP1CPSR_CPSDVSR_DIV2;
}

/**************************************************************************/
/*!
    Set SSP clock to fast mode
*/
/**************************************************************************/
static void FCLK_FAST()
{
    /* Divide by 1 (SSPCLKDIV also enables to SSP CLK) */
    SCB_SSP1CLKDIV = SCB_SSP1CLKDIV_DIV1;

    /* (PCLK / (CPSDVSR * [SCR+1])) = (36,000,000 / (2 x [8 + 1])) = 2.0 MHz */
    uint32_t configReg = ( SSP_SSP1CR0_DSS_8BIT   // Data size = 8-bit
                  | SSP_SSP1CR0_FRF_SPI           // Frame format = SPI
                  | SSP_SSP1CR0_SCR_8);           // Serial clock rate = 8

    // Set clock polarity (low between frames)
    // configReg &= ~SSP_SSP1CR0_CPOL_MASK;
    // configReg |= SSP_SSP1CR0_CPOL_LOW;

    // Set edge transition (leading edge)
    // configReg &= ~SSP_SSP1CR0_CPHA_MASK;
    // configReg |= SSP_SSP1CR0_CPHA_FIRST;

    // Assign config values to SSP1CR0
    SSP_SSP1CR0 = configReg;

    /* Clock prescale register must be even and at least 2 in master mode */
    SSP_SSP1CPSR = SSP_SSP1CPSR_CPSDVSR_DIV2;
}


/*--------------------------------------------------------------------------

   Module Private Functions

---------------------------------------------------------------------------*/




/* MMC/SD command */
#define CMD0(0)/* GO_IDLE_STATE */
#define CMD1(1)/* SEND_OP_COND (MMC) */
#defineACMD41(0x80+41)/* SEND_OP_COND (SDC) */
#define CMD8(8)/* SEND_IF_COND */
#define CMD9(9)/* SEND_CSD */
#define CMD10(10)/* SEND_CID */
#define CMD12(12)/* STOP_TRANSMISSION */
#define ACMD13(0x80+13)/* SD_STATUS (SDC) */
#define CMD16(16)/* SET_BLOCKLEN */
#define CMD17(17)/* READ_SINGLE_BLOCK */
#define CMD18(18)/* READ_MULTIPLE_BLOCK */
#define CMD23(23)/* SET_BLOCK_COUNT (MMC) */
#defineACMD23(0x80+23)/* SET_WR_BLK_ERASE_COUNT (SDC) */
#define CMD24(24)/* WRITE_BLOCK */
#define CMD25(25)/* WRITE_MULTIPLE_BLOCK */
#define CMD32(32)/* ERASE_ER_BLK_START */
#define CMD33(33)/* ERASE_ER_BLK_END */
#define CMD38(38)/* ERASE */
#define CMD55(55)/* APP_CMD */
#define CMD58(58)/* READ_OCR */


static volatile
DSTATUS Stat = STA_NOINIT;/* Physical drive status */

static volatile
UINT Timer1, Timer2;/* 1kHz decrement timer stopped at zero (disk_timerproc()) */

static
BYTE CardType;/* Card type flags */

/* Card type flags (CardType) */
#define CT_MMC0x01/* MMC ver 3 */
#define CT_SD10x02/* SD ver 1 */
#define CT_SD20x04/* SD ver 2 */
#define CT_SDC(CT_SD1|CT_SD2)/* SD */
#define CT_BLOCK0x08/* Block addressing */

DWORD get_fattime(void)
{
return 0;
}

/*-----------------------------------------------------------------------*/
/* Send/Receive data to the MMC  (Platform dependent)                    */
/*-----------------------------------------------------------------------*/

/* Exchange a byte */
static
BYTE xchg_spi (
BYTE dat/* Data to send */
)
{
SSPxDR = dat;
while (SSPxSR & 0x10) ;
return SSPxDR;
}


/* Receive multiple byte */
static
void rcvr_spi_multi (
BYTE *buff,/* Pointer to data buffer */
UINT btr/* Number of bytes to receive (16, 64 or 512) */
)
{
UINT n = 512;
WORD d;


SSPxCR0 = 0x000F;/* Select 16-bit mode */

for (n = 0; n < 8; n++)/* Push 8 frames into pipeline  */
SSPxDR = 0xFFFF;
btr -= 16;
while (btr) {/* Receive the data block into buffer */
while (!(SSPxSR & (1<<2))) ;
d = SSPxDR;
SSPxDR = 0xFFFF;
*buff++ = d >> 8;
*buff++ = d;
btr -= 2;
}
for (n = 0; n < 8; n++) {/* Pop remaining frames from pipeline */
while (!(SSPxSR & (1<<2))) ;
d = SSPxDR;
*buff++ = d >> 8;
*buff++ = d;
}

SSPxCR0 = 0x0007;/* Select 8-bit mode */
}


//#if _USE_WRITE
/* Send multiple byte */
static
void xmit_spi_multi (
const BYTE *buff,/* Pointer to the data */
UINT btx/* Number of bytes to send (512) */
)
{
UINT n = 512;
WORD d;


SSPxCR0 = 0x000F;/* Select 16-bit mode */

for (n = 0; n < 8; n++) {/* Push 8 frames into pipeline  */
d = *buff++;
d = (d << 8) | *buff++;
SSPxDR = d;
}
btx -= 16;
do {/* Transmit data block */
d = *buff++;
d = (d << 8) | *buff++;
while (!(SSPxSR & (1<<2))) ;
SSPxDR; SSPxDR = d;
} while (btx -= 2);
for (n = 0; n < 8; n++) {
while (!(SSPxSR & (1<<2))) ;
SSPxDR;
}

SSPxCR0 = 0x0007;/* Select 8-bit mode */
}
//#endif


/*-----------------------------------------------------------------------*/
/* Wait for card ready                                                   */
/*-----------------------------------------------------------------------*/

static
int wait_ready (/* 1:Ready, 0:Timeout */
UINT wt/* Timeout [ms] */
)
{
BYTE d;


Timer2 = wt;
do {
d = xchg_spi(0xFF);
/* This loop takes a time. Insert rot_rdq() here for multitask envilonment. */
} while (d != 0xFF && Timer2);/* Wait for card goes ready or timeout */

return (d == 0xFF) ? 1 : 0;
}



/*-----------------------------------------------------------------------*/
/* Deselect card and release SPI                                         */
/*-----------------------------------------------------------------------*/

static
void deselect (void)
{
CS_HIGH();/* CS = H */
xchg_spi(0xFF);/* Dummy clock (force DO hi-z for multiple slave SPI) */

}



/*-----------------------------------------------------------------------*/
/* Select card and wait for ready                                        */
/*-----------------------------------------------------------------------*/

static
int select (void)/* 1:OK, 0:Timeout */
{
CS_LOW();
xchg_spi(0xFF);/* Dummy clock (force DO enabled) */

if (wait_ready(500)) return 1;/* OK */
deselect();
return 0;/* Timeout */
}



/*-----------------------------------------------------------------------*/
/* Control SPI module (Platform dependent)                               */
/*-----------------------------------------------------------------------*/

static
void power_on (void)/* Enable SSP module and attach it to I/O pads */
{/*
__set_PCONP(PCSSPx, 1);// Enable SSP module
__set_PCLKSEL(PCLKSSPx, PCLKDIV_SSP);// Select PCLK frequency for SSP
SSPxCR0 = 0x0007;// Set mode: SPI mode 0, 8-bit
SSPxCR1 = 0x2;// Enable SSP with Master
#if SSP_CH == 0
__set_PINSEL(0, 15, 2);// Attach SCK0 to I/O pad
__set_PINSEL(0, 16, 2);// Attach MISO0 to I/O pad
__set_PINSEL(0, 17, 2);// Attach MOSI0 to I/O pad
FIO0DIR |= _BV(18);// Set CS# as output
#elif SSP_CH == 1
__set_PINSEL(0, 7, 2);// Attach SCK1 to I/O pad
__set_PINSEL(0, 8, 2);// Attach MISO1 to I/O pad
__set_PINSEL(0, 9, 2);// Attach MOSI1 to I/O pad
FIO0DIR |= _BV(6);// Set CS# as output
#endif*/

init_spi();
CS_HIGH();// Set CS# high

//for (Timer1 = 10; Timer1; ) ;/* 10ms */
}


static
void power_off (void)/* Disable SPI function */
{
select();/* Wait for card ready */
deselect();
}



/*-----------------------------------------------------------------------*/
/* Receive a data packet from the MMC                                    */
/*-----------------------------------------------------------------------*/

static
int rcvr_datablock (/* 1:OK, 0:Error */
BYTE *buff,/* Data buffer */
UINT btr/* Data block length (byte) */
)
{
BYTE token;


Timer1 = 200;
do {/* Wait for DataStart token in timeout of 200ms */
token = xchg_spi(0xFF);
/* This loop will take a time. Insert rot_rdq() here for multitask envilonment. */
} while ((token == 0xFF) && Timer1);
if(token != 0xFE) return 0;/* Function fails if invalid DataStart token or timeout */

rcvr_spi_multi(buff, btr);/* Store trailing data to the buffer */
xchg_spi(0xFF); xchg_spi(0xFF);/* Discard CRC */

return 1;/* Function succeeded */
}



/*-----------------------------------------------------------------------*/
/* Send a data packet to the MMC                                         */
/*-----------------------------------------------------------------------*/

//#if _USE_WRITE
static
int xmit_datablock (/* 1:OK, 0:Failed */
const BYTE *buff,/* Ponter to 512 byte data to be sent */
BYTE token/* Token */
)
{
BYTE resp;


if (!wait_ready(500)) return 0;/* Wait for card ready */

xchg_spi(token);/* Send token */
if (token != 0xFD) {/* Send data if token is other than StopTran */
xmit_spi_multi(buff, 512);/* Data */
xchg_spi(0xFF); xchg_spi(0xFF);/* Dummy CRC */

resp = xchg_spi(0xFF);/* Receive data resp */
if ((resp & 0x1F) != 0x05)/* Function fails if the data packet was not accepted */
return 0;
}
return 1;
}
//#endif


/*-----------------------------------------------------------------------*/
/* Send a command packet to the MMC                                      */
/*-----------------------------------------------------------------------*/

static
BYTE send_cmd (/* Return value: R1 resp (bit7==1:Failed to send) */
BYTE cmd,/* Command index */
DWORD arg/* Argument */
)
{
BYTE n, res;


if (cmd & 0x80) {/* Send a CMD55 prior to ACMD<n> */
cmd &= 0x7F;
res = send_cmd(CMD55, 0);
if (res > 1) return res;
}

/* Select card */
deselect();
if (!select()) return 0xFF;

/* Send command packet */
xchg_spi(0x40 | cmd);/* Start + command index */
xchg_spi((BYTE)(arg >> 24));/* Argument[31..24] */
xchg_spi((BYTE)(arg >> 16));/* Argument[23..16] */
xchg_spi((BYTE)(arg >> 8));/* Argument[15..8] */
xchg_spi((BYTE)arg);/* Argument[7..0] */
n = 0x01;/* Dummy CRC + Stop */
if (cmd == CMD0) n = 0x95;/* Valid CRC for CMD0(0) */
if (cmd == CMD8) n = 0x87;/* Valid CRC for CMD8(0x1AA) */
xchg_spi(n);

/* Receive command resp */
if (cmd == CMD12) xchg_spi(0xFF);/* Diacard following one byte when CMD12 */
n = 10;/* Wait for response (10 bytes max) */
do
res = xchg_spi(0xFF);
while ((res & 0x80) && --n);

return res;/* Return received response */
}



/*--------------------------------------------------------------------------

   Public Functions

---------------------------------------------------------------------------*/


/*-----------------------------------------------------------------------*/
/* Initialize disk drive                                                 */
/*-----------------------------------------------------------------------*/

DSTATUS disk_initialize (
BYTE drv/* Physical drive number (0) */
)
{
BYTE n, cmd, ty, ocr[4];


if (drv) return STA_NOINIT;/* Supports only drive 0 */
power_on();/* Initialize SPI */

if (Stat & STA_NODISK) return Stat;/* Is card existing in the soket? */

FCLK_SLOW();
for (n = 10; n; n--) xchg_spi(0xFF);/* Send 80 dummy clocks */

ty = 0;
if (send_cmd(CMD0, 0) == 1) {/* Put the card SPI/Idle state */
Timer1 = 1000;/* Initialization timeout = 1 sec */
if (send_cmd(CMD8, 0x1AA) == 1) {/* SDv2? */
for (n = 0; n < 4; n++) ocr[n] = xchg_spi(0xFF);/* Get 32 bit return value of R7 resp */
if (ocr[2] == 0x01 && ocr[3] == 0xAA) {/* Is the card supports vcc of 2.7-3.6V? */
while (Timer1 && send_cmd(ACMD41, 1UL << 30)) ;/* Wait for end of initialization with ACMD41(HCS) */
if (Timer1 && send_cmd(CMD58, 0) == 0) {/* Check CCS bit in the OCR */
for (n = 0; n < 4; n++) ocr[n] = xchg_spi(0xFF);
ty = (ocr[0] & 0x40) ? CT_SD2 | CT_BLOCK : CT_SD2;/* Card id SDv2 */
}
}
} else {/* Not SDv2 card */
if (send_cmd(ACMD41, 0) <= 1) {/* SDv1 or MMC? */
ty = CT_SD1; cmd = ACMD41;/* SDv1 (ACMD41(0)) */
} else {
ty = CT_MMC; cmd = CMD1;/* MMCv3 (CMD1(0)) */
}
while (Timer1 && send_cmd(cmd, 0)) ;/* Wait for end of initialization */
if (!Timer1 || send_cmd(CMD16, 512) != 0)/* Set block length: 512 */
ty = 0;
}
}
CardType = ty;/* Card type */
deselect();

if (ty) {/* OK */
FCLK_FAST();/* Set fast clock */
Stat &= ~STA_NOINIT;/* Clear STA_NOINIT flag */
} else {/* Failed */
power_off();
Stat = STA_NOINIT;
}

return Stat;
}



/*-----------------------------------------------------------------------*/
/* Get disk status                                                       */
/*-----------------------------------------------------------------------*/

DSTATUS disk_status (
BYTE drv/* Physical drive number (0) */
)
{
if (drv) return STA_NOINIT;/* Supports only drive 0 */

return Stat;/* Return disk status */
}



/*-----------------------------------------------------------------------*/
/* Read sector(s)                                                        */
/*-----------------------------------------------------------------------*/

DRESULT disk_read (
BYTE drv,/* Physical drive number (0) */
BYTE *buff,/* Pointer to the data buffer to store read data */
DWORD sector,/* Start sector number (LBA) */
BYTE count/* Number of sectors to read (1..128) */
)
{
if (drv || !count) return RES_PARERR;/* Check parameter */
if (Stat & STA_NOINIT) return RES_NOTRDY;/* Check if drive is ready */

if (!(CardType & CT_BLOCK)) sector *= 512;/* LBA ot BA conversion (byte addressing cards) */

if (count == 1) {/* Single sector read */
if ((send_cmd(CMD17, sector) == 0)/* READ_SINGLE_BLOCK */
&& rcvr_datablock(buff, 512))
count = 0;
}
else {/* Multiple sector read */
if (send_cmd(CMD18, sector) == 0) {/* READ_MULTIPLE_BLOCK */
do {
if (!rcvr_datablock(buff, 512)) break;
buff += 512;
} while (--count);
send_cmd(CMD12, 0);/* STOP_TRANSMISSION */
}
}
deselect();

return count ? RES_ERROR : RES_OK;/* Return result */
}



/*-----------------------------------------------------------------------*/
/* Write sector(s)                                                       */
/*-----------------------------------------------------------------------*/

//#if _USE_WRITE
DRESULT disk_write (
BYTE drv,/* Physical drive number (0) */
const BYTE *buff,/* Ponter to the data to write */
DWORD sector,/* Start sector number (LBA) */
BYTE count/* Number of sectors to write (1..128) */
)
{
if (drv || !count) return RES_PARERR;/* Check parameter */
if (Stat & STA_NOINIT) return RES_NOTRDY;/* Check drive status */
if (Stat & STA_PROTECT) return RES_WRPRT;/* Check write protect */

if (!(CardType & CT_BLOCK)) sector *= 512;/* LBA ==> BA conversion (byte addressing cards) */

if (count == 1) {/* Single sector write */
if ((send_cmd(CMD24, sector) == 0)/* WRITE_BLOCK */
&& xmit_datablock(buff, 0xFE))
count = 0;
}
else {/* Multiple sector write */
if (CardType & CT_SDC) send_cmd(ACMD23, count);/* Predefine number of sectors */
if (send_cmd(CMD25, sector) == 0) {/* WRITE_MULTIPLE_BLOCK */
do {
if (!xmit_datablock(buff, 0xFC)) break;
buff += 512;
} while (--count);
if (!xmit_datablock(0, 0xFD))/* STOP_TRAN token */
count = 1;
}
}
deselect();

return count ? RES_ERROR : RES_OK;/* Return result */
}
//#endif


/*-----------------------------------------------------------------------*/
/* Miscellaneous drive controls other than data read/write               */
/*-----------------------------------------------------------------------*/

#if _USE_IOCTL
DRESULT disk_ioctl (
BYTE drv,/* Physical drive number (0) */
BYTE cmd,/* Control command code */
void *buff/* Pointer to the conrtol data */
)
{
DRESULT res;
BYTE n, csd[16], *ptr = buff;
DWORD *dp, st, ed, csize;


if (drv) return RES_PARERR;/* Check parameter */
if (Stat & STA_NOINIT) return RES_NOTRDY;/* Check if drive is ready */

res = RES_ERROR;

switch (cmd) {
case CTRL_SYNC :/* Wait for end of internal write process of the drive */
if (select()) res = RES_OK;
break;

case GET_SECTOR_COUNT :/* Get drive capacity in unit of sector (DWORD) */
if ((send_cmd(CMD9, 0) == 0) && rcvr_datablock(csd, 16)) {
if ((csd[0] >> 6) == 1) {/* SDC ver 2.00 */
csize = csd[9] + ((WORD)csd[8] << 8) + ((DWORD)(csd[7] & 63) << 16) + 1;
*(DWORD*)buff = csize << 10;
} else {/* SDC ver 1.XX or MMC ver 3 */
n = (csd[5] & 15) + ((csd[10] & 128) >> 7) + ((csd[9] & 3) << 1) + 2;
csize = (csd[8] >> 6) + ((WORD)csd[7] << 2) + ((WORD)(csd[6] & 3) << 10) + 1;
*(DWORD*)buff = csize << (n - 9);
}
res = RES_OK;
}
break;

case GET_SECTOR_SIZE :/* Get sector size in unit of byte (WORD) */
*(WORD*)buff = 512;
res = RES_OK;
break;

case GET_BLOCK_SIZE :/* Get erase block size in unit of sector (DWORD) */
if (CardType & CT_SD2) {/* SDC ver 2.00 */
if (send_cmd(ACMD13, 0) == 0) {/* Read SD status */
xchg_spi(0xFF);
if (rcvr_datablock(csd, 16)) {/* Read partial block */
for (n = 64 - 16; n; n--) xchg_spi(0xFF);/* Purge trailing data */
*(DWORD*)buff = 16UL << (csd[10] >> 4);
res = RES_OK;
}
}
} else {/* SDC ver 1.XX or MMC */
if ((send_cmd(CMD9, 0) == 0) && rcvr_datablock(csd, 16)) {/* Read CSD */
if (CardType & CT_SD1) {/* SDC ver 1.XX */
*(DWORD*)buff = (((csd[10] & 63) << 1) + ((WORD)(csd[11] & 128) >> 7) + 1) << ((csd[13] >> 6) - 1);
} else {/* MMC */
*(DWORD*)buff = ((WORD)((csd[10] & 124) >> 2) + 1) * (((csd[11] & 3) << 3) + ((csd[11] & 224) >> 5) + 1);
}
res = RES_OK;
}
}
break;

case CTRL_ERASE_SECTOR :/* Erase a block of sectors (used when _USE_ERASE == 1) */
if (!(CardType & CT_SDC)) break;/* Check if the card is SDC */
if (disk_ioctl(drv, MMC_GET_CSD, csd)) break;/* Get CSD */
if (!(csd[0] >> 6) && !(csd[10] & 0x40)) break;/* Check if sector erase can be applied to the card */
dp = buff; st = dp[0]; ed = dp[1];/* Load sector block */
if (!(CardType & CT_BLOCK)) {
st *= 512; ed *= 512;
}
if (send_cmd(CMD32, st) == 0 && send_cmd(CMD33, ed) == 0 && send_cmd(CMD38, 0) == 0 && wait_ready(30000))/* Erase sector block */
res = RES_OK;/* FatFs does not check result of this command */
break;

/* Following commands are never used by FatFs module */

case MMC_GET_TYPE :/* Get MMC/SDC type (BYTE) */
*ptr = CardType;
res = RES_OK;
break;

case MMC_GET_CSD :/* Read CSD (16 bytes) */
if (send_cmd(CMD9, 0) == 0/* READ_CSD */
&& rcvr_datablock(ptr, 16))
res = RES_OK;
break;

case MMC_GET_CID :/* Read CID (16 bytes) */
if (send_cmd(CMD10, 0) == 0/* READ_CID */
&& rcvr_datablock(ptr, 16))
res = RES_OK;
break;

case MMC_GET_OCR :/* Read OCR (4 bytes) */
if (send_cmd(CMD58, 0) == 0) {/* READ_OCR */
for (n = 4; n; n--) *ptr++ = xchg_spi(0xFF);
res = RES_OK;
}
break;

case MMC_GET_SDSTAT :/* Read SD status (64 bytes) */
if (send_cmd(ACMD13, 0) == 0) {/* SD_STATUS */
xchg_spi(0xFF);
if (rcvr_datablock(ptr, 64))
res = RES_OK;
}
break;

default:
res = RES_PARERR;
}

deselect();

return res;
}
#endif


/*-----------------------------------------------------------------------*/
/* Device timer function                                                 */
/*-----------------------------------------------------------------------*/
/* This function must be called from timer interrupt routine in period
/  of 1 ms to generate card control timing.
*/

void disk_timerproc (void)
{
WORD n;
BYTE s;


n = Timer1;/* 1kHz decrement timer stopped at 0 */
if (n) Timer1 = --n;
n = Timer2;
if (n) Timer2 = --n;

s = Stat;
if (WP)/* Write protected */
s |= STA_PROTECT;
else/* Write enabled */
s &= ~STA_PROTECT;
if (INS)/* Card is in socket */
s &= ~STA_NODISK;
else/* Socket empty */
s |= (STA_NODISK | STA_NOINIT);
Stat = s;
}


DWORD get_fattime (void)
{
return  ((DWORD)(2012 - 1980) << 25)/* Year = 2012 */
| ((DWORD)1 << 21)/* Month = 1 */
| ((DWORD)1 << 16)/* Day_m = 1*/
| ((DWORD)0 << 11)/* Hour = 0 */
| ((DWORD)0 << 5)/* Min = 0 */
| ((DWORD)0 >> 1);/* Sec = 0 */
}


SD won't mount right now, it looks like it can't detect a card. I know there's a LPC1114 CodeBase that uses FatFs,but I'm close to giving up, so if someone can point out more or less obvious mistakes, or better yet, show some simple exlample projecto for lpc11xx, I would appreciate that...
Labels (1)
0 Kudos
Reply
0 Replies