lpc-link2 for lpc811

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc-link2 for lpc811

1,800 Views
herusetiawan
Contributor II

Dear NXP Team,

I just buy lpc-link2. I have plan to use it for programming and debugging lpc811m001jdh16.

Any configuration needed in MCUXpresso if I use SWD for programming and debugging?

if I see on lpc-link2, have J8, J7,J2 those all support SWD. Can I choose J8/J7/J2 free?

Please advice,

Thanks

Labels (1)
1 Reply

1,653 Views
lpcxpresso_supp
NXP Employee
NXP Employee

To debug your target MCU, connect the a USB cable from your PC to the LPC-Link2 and the supplied 10-pin debug cable from the J7 connector (Target SWD/JTG) to the target board.

There is also information on designing a board for debug compatibility at: Design Considerations for Debug 

For more information on using LPC-Link2 with MCUXpresso IDE, please see the MCUXpresso IDE v10.1 User Guide, which can be downloaded from : http://www.nxp.com/mcuxpresso/ide/documentation.

For assistance on using MCUXpresso IDE, visit the MCUXpresso IDE community :MCUXpresso IDE 

Regards,

MCUXpresso IDE Support