lpc 433x DFU script for RASPBERRY 3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

lpc 433x DFU script for RASPBERRY 3

跳至解决方案
2,184 次查看
vianneyfenart
Contributor II

Hello,

I want upload bin file from RASPBERRY 3 (RASPBIAN) to LPC433X ARM processor in dfu mode.

I can do that easily with dfusec utility on Windows but i can't find the equivalent for a ARM LINUX OS...

Have you got solution?

thanks

标签 (2)
1 解答
2,037 次查看
bernhardfink
NXP Employee
NXP Employee

For Linux there is a DFU utility called dfu-util:   dfu-util Homepage 

But it's not a dedicated flash utility for the LPC1800/4300 platform.

NXP has a tool for Linux which should do what you want:    LPCScrypt v1.8.2|NXP 

在原帖中查看解决方案

2 回复数
2,038 次查看
bernhardfink
NXP Employee
NXP Employee

For Linux there is a DFU utility called dfu-util:   dfu-util Homepage 

But it's not a dedicated flash utility for the LPC1800/4300 platform.

NXP has a tool for Linux which should do what you want:    LPCScrypt v1.8.2|NXP 

2,037 次查看
vianneyfenart
Contributor II

Thanks for your help!

0 项奖励
回复