load SBKEK with application ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

load SBKEK with application ?

1,314 Views
slou26
Contributor II

Hello, Today in ISP mode we use the rom bootloader key provisionning command ( blhost -p com6 -- key-provisioning set_user_key 3 sbkek.bin ) to load the sbkek into the keystore , and it's works fine . But in the future, this operation will not be possible because of Isp disabled , so we have to do this operation with an application , is it possible ? Can I use the FFR_KeystoreWrite function and how ? Thanks for your help . Regards,

0 Kudos
Reply
1 Reply

1,250 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Sebastien,

 

First of all, please accept my apologies for my late reply. We have been under a big workload. Could you please clarify the MCU you are working on?

 

Typically,  FFR_KeystoreWrite are IAP functions so you do not have to worry if you disable ISP on your MCU. In Application Programming allows application software for programming and reading the flash memory in addition to other functions.

 

Best regards,

Felipe

0 Kudos
Reply