linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux

2,074件の閲覧回数
hiromasashigema
Contributor II

I am now using the LPC1830 on Windows10 by the interface of lpc_dfusec tool.

Can I use the LPC1830 on Linux by the interface of lpc_dfusec tool.

If you give me any comment for my question, I am very happy.

Shiggy

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,828件の閲覧回数
thefallguy
Contributor IV

Lpc_dfusec is a Windows tool only.

use LPCScrypt v1.8.0|NXP instead, which works on Windows, Linux, and Mac.

0 件の賞賛
返信

1,828件の閲覧回数
hiromasashigema
Contributor II

Hi dear sir!

Thanks your good new for me.

>use LPCScrypt v1.8.0|NXP

<https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fsoftware-development-tools%2Fsoftware-tools%2Flpc-microcontroller-utilities%2Flpcscrypt-v1.8.0%3ALPCSCRYPT>

instead,

which works on Windows, Linux, and Mac.

<---I have already checke LPCScrypt v1.8.0|NXP

<https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fsoftware-development-tools%2Fsoftware-tools%2Flpc-microcontroller-utilities%2Flpcscrypt-v1.8.0%3ALPCSCRYPT>

, so the LPC1830 works on Linux, instead of Windows.

Thanks your important information for me.

Shiggy

2017-03-17 17:08 GMT+09:00 thefallguy <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: linux

reply from Fall Guy

<https://community.nxp.com/people/thefallguy?et=watches.email.thread> in

LPC - View the full discussion

<https://community.nxp.com/message/887909?commentID=887909&et=watches.email.thread#comment-887909>

0 件の賞賛
返信