linkserver not found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,175件の閲覧回数
edelbertgreiner
Contributor I

I was working with the LPC54102 on OM13077 for many weeks.

Emulator functions were working well all the time.

Today, I can't get connection to the emulator. This makes it impossible for me

to continue working with the Project.

Connect to emulator: LinkServer

LinkServer not found.

Search for any enabled emulator

No compatible emulators available

I am sure that the connections are made, becaus my software is runnung

on OM13077 and LED is blinking. No emulator is recognised by the software, but the emulator

is still here on my table and all necessary connections are made.

ラベル(2)
1 解決策
3,071件の閲覧回数
edelbertgreiner
Contributor I

After changing USB-Connection from HUB to PC directly, it worked.

Therfore I am looking for a software- update for the HUB or a new HUB.

元の投稿で解決策を見る

2 返答(返信)
3,072件の閲覧回数
edelbertgreiner
Contributor I

After changing USB-Connection from HUB to PC directly, it worked.

Therfore I am looking for a software- update for the HUB or a new HUB.

3,071件の閲覧回数
soledad
NXP Employee
NXP Employee

Thank you for your input. 

Have a nice day!

0 件の賞賛
返信