kSCTIMER_Out_* doesn't work except for kSCTIMER_Out_2 and kSCTIMER_Out_4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kSCTIMER_Out_* doesn't work except for kSCTIMER_Out_2 and kSCTIMER_Out_4

Jump to solution
1,773 Views
jren68
Contributor III

I am looking at the sctimer_simple_pwm example provided for lpc54018.

According to the pin table for UM11079. for J11 area, the Sctimer output and pin correspondence are

Index Pin  SCTimer_OUT

1       2_2    6

2       3_28  2

3       3_14  4

4       3_10  3

....

The provided example is

#define DEMO_FIRST_SCTIMER_OUT kSCTIMER_Out_4

#define DEMO_SECOND_SCTIMER_OUT kSCTIMER_Out_2

int main(void)

{

    sctimer_config_t sctimerInfo;

    sctimer_pwm_signal_param_t pwmParam;

    uint32_t event;

    uint32_t sctimerClock;

    /* Board pin, clock, debug console init */

    /* attach 12 MHz clock to FLEXCOMM0 (debug console) */

    CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);

    BOARD_InitPins();

    BOARD_BootClockFROHF96M();

    BOARD_InitDebugConsole();

    sctimerClock = SCTIMER_CLK_FREQ;

    SCTIMER_GetDefaultConfig(&sctimerInfo);

    /* Initialize SCTimer module */

    SCTIMER_Init(SCT0, &sctimerInfo);

    /* Configure first PWM with frequency 24kHZ from first output */

    pwmParam.output = DEMO_FIRST_SCTIMER_OUT;

    pwmParam.level = kSCTIMER_HighTrue;

    pwmParam.dutyCyclePercent = 50;

    if (SCTIMER_SetupPwm(SCT0, &pwmParam, kSCTIMER_CenterAlignedPwm, 24000U, sctimerClock, &event) == kStatus_Fail)

    {

        return -1;

    }

    /* Configure second PWM with different duty cycle but same frequency as before */

    pwmParam.output = DEMO_SECOND_SCTIMER_OUT;

    pwmParam.level = kSCTIMER_LowTrue;

    pwmParam.dutyCyclePercent = 20;

    if (SCTIMER_SetupPwm(SCT0, &pwmParam, kSCTIMER_CenterAlignedPwm, 24000U, sctimerClock, &event) == kStatus_Fail)

    {

        return -1;

    }

    /* Start the timer */

    SCTIMER_StartTimer(SCT0, kSCTIMER_Counter_L);

    while (1)

    {

    }

}

And it worked.

However, if I change kSCTIMER_Out_4 into kSCTIMER_Out_6 or kSCTIMER_Out_3, and plug the LED into the corresponding pinholes, the LED is not flickering.

Why only kSCTIMER_Out_4 and kSCTIMER_Out_2 works? How may I use the rest of the pinholes? (I need a third pinhole to PWM a tricolor LED)

Thanks,

Jenny

Labels (1)
1 Solution
1,636 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jenny,

   Yes, if you want to change the STC output pin, you also need to modify the pin_mux BOARD_InitPins function.

   You need to define P2_2 and P3_10 FUNC to SCT output function.

   So, now, when you define the according pin configuration, do you make it works?

  const uint32_t port2_pin2_config = (
    IOCON_PIO_FUNC3 |                                        /* Pin is configured as SCT0_OUT4 */
    IOCON_PIO_MODE_INACT |                                   /* No addition pin function */
    IOCON_PIO_INV_DI |                                       /* Input function is not inverted */
    IOCON_PIO_DIGITAL_EN |                                   /* Enables digital function */
    IOCON_PIO_INPFILT_OFF |                                  /* Input filter disabled */
    IOCON_PIO_SLEW_STANDARD |                                /* Standard mode, output slew rate control is enabled */
    IOCON_PIO_OPENDRAIN_DI                                   /* Open drain is disabled */
  );
  IOCON_PinMuxSet(IOCON, 2u, 2u, port2_pin2_config );
  const uint32_t port3_pin10_config = (
    IOCON_PIO_FUNC1 |                                        /* Pin is configured as SCT0_OUT2 */
    IOCON_PIO_MODE_INACT |                                   /* No addition pin function */
    IOCON_PIO_INV_DI |                                       /* Input function is not inverted */
    IOCON_PIO_DIGITAL_EN |                                   /* Enables digital function */
    IOCON_PIO_INPFILT_OFF |                                  /* Input filter disabled */
    IOCON_PIO_SLEW_STANDARD |                                /* Standard mode, output slew rate control is enabled */
    IOCON_PIO_OPENDRAIN_DI                                   /* Open drain is disabled */
  );
  IOCON_PinMuxSet(IOCON, PORT3_IDX, 10u, port3_pin10_config );

If you still have problem about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,636 Views
jren68
Contributor III

It turns out in the board/src/pin_mux

in BOARD_InitPins()

you need to define something like 

port2_pin2_config if you wanna use the SCTimer_out_6 P2_2 correspond to

check line 120-140 for examples of P3_14 (SCTimer_out_4) and P3_28(SCTimer_out_2)

0 Kudos
Reply
1,637 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jenny,

   Yes, if you want to change the STC output pin, you also need to modify the pin_mux BOARD_InitPins function.

   You need to define P2_2 and P3_10 FUNC to SCT output function.

   So, now, when you define the according pin configuration, do you make it works?

  const uint32_t port2_pin2_config = (
    IOCON_PIO_FUNC3 |                                        /* Pin is configured as SCT0_OUT4 */
    IOCON_PIO_MODE_INACT |                                   /* No addition pin function */
    IOCON_PIO_INV_DI |                                       /* Input function is not inverted */
    IOCON_PIO_DIGITAL_EN |                                   /* Enables digital function */
    IOCON_PIO_INPFILT_OFF |                                  /* Input filter disabled */
    IOCON_PIO_SLEW_STANDARD |                                /* Standard mode, output slew rate control is enabled */
    IOCON_PIO_OPENDRAIN_DI                                   /* Open drain is disabled */
  );
  IOCON_PinMuxSet(IOCON, 2u, 2u, port2_pin2_config );
  const uint32_t port3_pin10_config = (
    IOCON_PIO_FUNC1 |                                        /* Pin is configured as SCT0_OUT2 */
    IOCON_PIO_MODE_INACT |                                   /* No addition pin function */
    IOCON_PIO_INV_DI |                                       /* Input function is not inverted */
    IOCON_PIO_DIGITAL_EN |                                   /* Enables digital function */
    IOCON_PIO_INPFILT_OFF |                                  /* Input filter disabled */
    IOCON_PIO_SLEW_STANDARD |                                /* Standard mode, output slew rate control is enabled */
    IOCON_PIO_OPENDRAIN_DI                                   /* Open drain is disabled */
  );
  IOCON_PinMuxSet(IOCON, PORT3_IDX, 10u, port3_pin10_config );

If you still have problem about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------