is42s16800

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is42s16800

1,389 Views
christianpeterk
Contributor I

Using LPC54605 and connected a SDRAM: is42s16800, and using MCUXpresso. Does any body have a working fsl_emc.c for that device?

0 Kudos
Reply
1 Reply

1,308 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Christian Peter Koch, 

Unfortunately, for that specific memory we don't have an example. The evaluation board for the LPC54608 comes with Winbond 128Mb W9812G6JB-6I SDRAM (Micron MT48LC8M16A2B4 used on all revisions up to Rev C and some Rev D.). You can use the example that we provide in the SDK for this evaluation board along with the following application note: https://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf as a starting point for your project with the memory is42s16800. If you find problems while developing this we will be happy to help you! 

Hope it helps! 

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply