interrupt produced when call Chip_UART_IntEnable()

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

interrupt produced when call Chip_UART_IntEnable()

1,170件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pmoreira on Mon Feb 23 12:56:47 MST 2015
Hi all,

Is normal that when I call the function Chip_UART_IntEnable(LPC_USART0, UART_INTEN_RXRDY) will produce an inmediate interrupt although don't exist data in serial port?

I am using LPC812, LPCXpresso v7.5.0 [Build 254] [2014-10-31] and LPC8xx UART driver.

Please, can anybody help me?

Many thanks in advance

pmoreira
ラベル(1)
0 件の賞賛
返信
1 返信

1,089件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Tue Feb 24 09:45:29 MST 2015
Hi pmoreira,

This isn't the first time I've seen this a situation where enabling an interrupt actually triggers the IRQ initially. Are you clearing all pending interrupts prior to enabling the UART interrupt? Does this "one time" interrupt affect your application negatively?
0 件の賞賛
返信