hwCAN_MsgTransmit fail with bit0error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hwCAN_MsgTransmit fail with bit0error

1,281件の閲覧回数
thomasjohansen
Contributor I


Hi,

 

Im using the sample "ccan_rom" from the lpcopn 2.20 with my own hardware platform.

The CAN high and low are located on pin 13 and 18. TJA1051 used.

 

But when I call the hwCAN_MsgTransmit i get an Bit0Error? I can't even moved the TD/RD pins in test mode?

The TJA1051 is connected correct..

 

Any idea's?

 

Thomas

タグ(1)
0 件の賞賛
返信
1 返信

1,129件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Thomas,

Could you tell us which LPC MCU are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信