how to see the output for usb example in lpc54628

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to see the output for usb example in lpc54628

Jump to solution
3,232 Views
Karthikeyan_J
Contributor II

hi

i am karthikeyan

I run the example program named USB HID Mouse application program. They said that this program will show a mouse ARROW moving on PC. I run this example in lpc54628 board, it was successfully build,clean& debug ,there was no error and warning.

But i not able to see the output in the PC , i tried with connecting a OTG cable in the USB port and with other end i connected the Mouse plug in OTG cable. I cant see the output the mouse cursor is not moving in my PC.

So my question is how to see the mouse arrow moving on the PC.

Thanking You,

Karthikeyan.

0 Kudos
Reply
1 Solution
3,221 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Please let me know your demo code name and version of SDK thus I will test it on my side.

There is an article, the hands on demo makes the mouse arrow moving on the PC screen in the rectangular rotation. The method is exactly the same for LPC54628

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-F...

 

Have a nice day,

Jun Zhang

View solution in original post

5 Replies
3,222 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Please let me know your demo code name and version of SDK thus I will test it on my side.

There is an article, the hands on demo makes the mouse arrow moving on the PC screen in the rectangular rotation. The method is exactly the same for LPC54628

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-F...

 

Have a nice day,

Jun Zhang

3,194 Views
Karthikeyan_J
Contributor II

Hi,

Zhang

I get the output.

Thank You.

can you tell me how the program is working, because i disconnected the mouse with the system but even though it still get square rotation. So my question is how the process taking place inside it(CPU & Microcontroller  LPC54628[OM13098] Board.

Thanking You,

Karthikeyan

0 Kudos
Reply
3,162 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

When you download dev_hid_mouse_bm to your demo board, the demo board is enumerated as a mouse. As long as you have the board connected, you will see rectangle rotation on the screen.

3,140 Views
Karthikeyan_J
Contributor II

Hi,

Zhang

Thank You

the below given code will help some person who search it,

#include "usb_device_config.h"
#include "usb.h"
#include "usb_device.h"
#include "usb_device_class.h"
#include "usb_device_hid.h"
#include "usb_device_ch9.h"
#include "usb_device_descriptor.h"
#include "mouse.h"
#include "fsl_device_registers.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_debug_console.h"
#include <stdio.h>
#include <stdlib.h>
#include "pin_mux.h"
#include <stdbool.h>
#include "fsl_power.h"
#include "fsl_mrt.h"
void BOARD_InitHardware(void);
void USB_DeviceClockInit(void);
void USB_DeviceIsrEnable(void);
static usb_status_t USB_DeviceHidMouseAction(void);//Update mouse pointer location. Draw a rectangular rotation
static usb_status_t USB_DeviceHidMouseCallback(class_handle_t handle, uint32_t event, void *param);//The hid class callback.send response if the device is attached
static usb_status_t USB_DeviceCallback(usb_device_handle handle, uint32_t event, void *param);//The device callback-Get hid physical descriptor request- USB bus reset signal detected-Set device configuration request-Set device interface request-Get current configuration request-Get device descriptor request-
static void USB_DeviceApplicationInit(void);// Initialize the usb stack and class drivers-Get the HID mouse class handle

uint32_t timerInterval;
uint32_t isConnectedToFsHost = 0U;
uint32_t isConnectedToHsHost = 0U;
USB_DMA_NONINIT_DATA_ALIGN(USB_DATA_ALIGN_SIZE) static uint8_t s_MouseBuffer[USB_HID_MOUSE_REPORT_LENGTH];
usb_hid_mouse_struct_t g_UsbDeviceHidMouse;

extern usb_device_class_struct_t g_UsbDeviceHidMouseConfig;

/* Set class configurations */
usb_device_class_config_struct_t g_UsbDeviceHidConfig[1] = {{
USB_DeviceHidMouseCallback, /* HID mouse class callback pointer */
(class_handle_t)NULL, /* The HID class handle, This field is set by USB_DeviceClassInit */
&g_UsbDeviceHidMouseConfig, /* The HID mouse configuration, including class code, subcode, and protocol, class type,
transfer type, endpoint address, max packet size, etc.*/
}};

/* Set class configuration list */
usb_device_class_config_list_struct_t g_UsbDeviceHidConfigList = {
g_UsbDeviceHidConfig, /* Class configurations */
USB_DeviceCallback, /* Device callback pointer */
1U, /* Class count */
};

/*******************************************************************************
* Code
******************************************************************************/
void USB_TimerInt(uint8_t instance, uint8_t enable)
{
MRT_Type *instanceList[] = MRT_BASE_PTRS;
uint32_t mrt_clock;
mrt_clock = CLOCK_GetFreq(kCLOCK_BusClk);
if (enable)
{
/* Start channel 0 */
MRT_StartTimer(instanceList[instance], kMRT_Channel_0, USEC_TO_COUNT(timerInterval, mrt_clock));
}
else
{
/* Stop channel 0 */
MRT_StopTimer(instanceList[instance], kMRT_Channel_0);
/* Clear interrupt flag.*/
MRT_ClearStatusFlags(instanceList[instance], kMRT_Channel_0, kMRT_TimerInterruptFlag);
}
}

void USB0_IRQHandler(void)
{
USB_DeviceLpcIp3511IsrFunction(g_UsbDeviceHidMouse.deviceHandle);
}

void USB_DeviceClockInit(void)
{

/* enable USB IP clock */
CLOCK_EnableUsbfs0DeviceClock(kCLOCK_UsbSrcFro, CLOCK_GetFroHfFreq());
for (int i = 0; i < FSL_FEATURE_USB_USB_RAM; i++)
{
((uint8_t *)FSL_FEATURE_USB_USB_RAM_BASE_ADDRESS)[i] = 0x00U;
}
}
void USB_DeviceIsrEnable(void)
{
uint8_t irqNumber;

uint8_t usbDeviceIP3511Irq[] = USB_IRQS;
irqNumber = usbDeviceIP3511Irq[CONTROLLER_ID - kUSB_ControllerLpcIp3511Fs0];
EnableIRQ((IRQn_Type)irqNumber);
}

/* Update mouse pointer location. Draw a rectangular rotation*/
static usb_status_t USB_DeviceHidMouseAction(void)
{
static int8_t x = 0U;
static int8_t y = 0U;
enum
{
RIGHT,
DOWN,
LEFT,
UP
};
static uint8_t dir = RIGHT;

switch (dir)
{
case RIGHT:
/* Move right. Increase X value. */
g_UsbDeviceHidMouse.buffer[1] = 2U;
g_UsbDeviceHidMouse.buffer[2] = 0U;
x++;
if (x > 99U)
{
dir++;
}
break;
case DOWN:
/* Move down. Increase Y value. */
g_UsbDeviceHidMouse.buffer[1] = 0U;
g_UsbDeviceHidMouse.buffer[2] = 2U;
y++;
if (y > 99U)
{
dir++;
}
break;
case LEFT:
/* Move left. Discrease X value. */
g_UsbDeviceHidMouse.buffer[1] = (uint8_t)(-2);
g_UsbDeviceHidMouse.buffer[2] = 0U;
x--;
if (x < 2U)
{
dir++;
}
break;
case UP:
/* Move up. Discrease Y value. */
g_UsbDeviceHidMouse.buffer[1] = 0U;
g_UsbDeviceHidMouse.buffer[2] = (uint8_t)(-2);
y--;
if (y < 2U)
{
dir = RIGHT;
}
break;
default:
break;
}
/* Send mouse report to the host */
return USB_DeviceHidSend(g_UsbDeviceHidMouse.hidHandle, USB_HID_MOUSE_ENDPOINT_IN, g_UsbDeviceHidMouse.buffer,
USB_HID_MOUSE_REPORT_LENGTH);
}

/* The hid class callback */
static usb_status_t USB_DeviceHidMouseCallback(class_handle_t handle, uint32_t event, void *param)
{
usb_status_t error = kStatus_USB_Error;
usb_device_endpoint_callback_message_struct_t *message = (usb_device_endpoint_callback_message_struct_t *)param;

switch (event)
{
case kUSB_DeviceHidEventSendResponse:
/* Resport sent */
if (g_UsbDeviceHidMouse.attach)
{
if ((NULL != message) && (message->length == USB_UNINITIALIZED_VAL_32))
{
return error;
}
error = USB_DeviceHidMouseAction();
}
}
}

/* The device callback */
static usb_status_t USB_DeviceCallback(usb_device_handle handle, uint32_t event, void *param)
{
usb_status_t error = kStatus_USB_Error;
uint16_t *temp16 = (uint16_t *)param;
uint8_t *temp8 = (uint8_t *)param;

switch (event)
{
case kUSB_DeviceEventBusReset:
{
/* USB bus reset signal detected */
g_UsbDeviceHidMouse.attach = 0U;
g_UsbDeviceHidMouse.currentConfiguration = 0U;
error = kStatus_USB_Success;
}
break;

case kUSB_DeviceEventSetConfiguration:
if (0U == (*temp8))
{
g_UsbDeviceHidMouse.attach = 0;
g_UsbDeviceHidMouse.currentConfiguration = 0U;
}
else if (USB_HID_MOUSE_CONFIGURE_INDEX == (*temp8))
{
/* Set device configuration request */
g_UsbDeviceHidMouse.attach = 1U;
g_UsbDeviceHidMouse.currentConfiguration = *temp8;
error = USB_DeviceHidMouseAction();
}
else
{
error = kStatus_USB_InvalidRequest;
}
break;
case kUSB_DeviceEventSetInterface:
if (g_UsbDeviceHidMouse.attach)
{
/* Set device interface request */
uint8_t interface = (uint8_t)((*temp16 & 0xFF00U) >> 0x08U);
uint8_t alternateSetting = (uint8_t)(*temp16 & 0x00FFU);
if (interface < USB_HID_MOUSE_INTERFACE_COUNT)
{
g_UsbDeviceHidMouse.currentInterfaceAlternateSetting[interface] = alternateSetting;
if (alternateSetting == 0U)
{
error = USB_DeviceHidMouseAction();
}
}
}
break;
case kUSB_DeviceEventGetConfiguration:
if (param)
{
/* Get current configuration request */
*temp8 = g_UsbDeviceHidMouse.currentConfiguration;
error = kStatus_USB_Success;
}
break;
case kUSB_DeviceEventGetInterface:
if (param)
{
/* Get current alternate setting of the interface request */
uint8_t interface = (uint8_t)((*temp16 & 0xFF00U) >> 0x08U);
if (interface < USB_HID_MOUSE_INTERFACE_COUNT)
{
*temp16 = (*temp16 & 0xFF00U) | g_UsbDeviceHidMouse.currentInterfaceAlternateSetting[interface];
error = kStatus_USB_Success;
}
else
{
error = kStatus_USB_InvalidRequest;
}
}
break;
case kUSB_DeviceEventGetDeviceDescriptor:
if (param)
{
/* Get device descriptor request */
error = USB_DeviceGetDeviceDescriptor(handle, (usb_device_get_device_descriptor_struct_t *)param);
}
break;
case kUSB_DeviceEventGetConfigurationDescriptor:
if (param)
{
/* Get device configuration descriptor request */
error = USB_DeviceGetConfigurationDescriptor(handle,
(usb_device_get_configuration_descriptor_struct_t *)param);
}
break;
case kUSB_DeviceEventGetStringDescriptor:
if (param)
{
/* Get device string descriptor request */
error = USB_DeviceGetStringDescriptor(handle, (usb_device_get_string_descriptor_struct_t *)param);
}
break;
case kUSB_DeviceEventGetHidDescriptor:
if (param)
{
/* Get hid descriptor request */
error = USB_DeviceGetHidDescriptor(handle, (usb_device_get_hid_descriptor_struct_t *)param);
}
break;
case kUSB_DeviceEventGetHidReportDescriptor:
if (param)
{
/* Get hid report descriptor request */
error =
USB_DeviceGetHidReportDescriptor(handle, (usb_device_get_hid_report_descriptor_struct_t *)param);
}
break;
case kUSB_DeviceEventGetHidPhysicalDescriptor:
if (param)
{
/* Get hid physical descriptor request */
error = USB_DeviceGetHidPhysicalDescriptor(handle,
(usb_device_get_hid_physical_descriptor_struct_t *)param);
}
break;
}
}
static void USB_DeviceApplicationInit(void)
{
USB_DeviceClockInit();
/* Set HID mouse to default state */
g_UsbDeviceHidMouse.speed = USB_SPEED_FULL;
g_UsbDeviceHidMouse.attach = 0U;
g_UsbDeviceHidMouse.hidHandle = (class_handle_t)NULL;
g_UsbDeviceHidMouse.deviceHandle = NULL;
g_UsbDeviceHidMouse.buffer = s_MouseBuffer;

/* Initialize the usb stack and class drivers */
if (kStatus_USB_Success !=
USB_DeviceClassInit(CONTROLLER_ID, &g_UsbDeviceHidConfigList, &g_UsbDeviceHidMouse.deviceHandle))
{
usb_echo("USB device mouse failed\r\n");
return;
}
else
{
usb_echo("USB device DCD + HID mouse demo\r\n");
usb_echo("USB device HID mouse demo\r\n");
/* Get the HID mouse class handle */
g_UsbDeviceHidMouse.hidHandle = g_UsbDeviceHidConfigList.config->classHandle;
}
USB_DeviceIsrEnable();
/*USB_DeviceRun could not be called here to avoid DP/DM confliction between DCD function and USB function in case
DCD is enabled. Instead, USB_DeviceRun should be called after the DCD is finished immediately*/
/* Start USB device HID mouse */
/*Add one delay here to make the DP pull down long enough to allow host to detect the previous disconnection.*/
SDK_DelayAtLeastUs(5000, SDK_DEVICE_MAXIMUM_CPU_CLOCK_FREQUENCY);
USB_DeviceRun(g_UsbDeviceHidMouse.deviceHandle);
}

/*!
* @brief Application task function.
*
* This function runs the task for application.
*
* @return None.
*/
void USB_DeviceAppTask(void *parameter)
{
usb_hid_mouse_struct_t *usbDeviceHid = (usb_hid_mouse_struct_t *)parameter;

if (usbDeviceHid->connectStateChanged)
{
usbDeviceHid->connectStateChanged = 0;
if (g_UsbDeviceHidMouse.connectState)
{
/*user need call USB_DeviceRun here to usb function run if dcd function is disabled*/
/*USB_DeviceRun(g_UsbDeviceHidMouse.deviceHandle);*/
usb_echo("USB device attached.\r\n");
}
else
{

usb_echo("USB device detached.\r\n");
}
}
}

void main(void)
{
/* attach 12 MHz clock to FLEXCOMM0 (debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);
BOARD_InitPins();
BOARD_BootClockFROHF96M();
BOARD_InitDebugConsole();
POWER_DisablePD(kPDRUNCFG_PD_USB0_PHY); /*< Turn on USB Phy */
CLOCK_SetClkDiv(kCLOCK_DivUsb0Clk, 1, false);
CLOCK_AttachClk(kFRO_HF_to_USB0_CLK);
/* enable usb0 host clock */
CLOCK_EnableClock(kCLOCK_Usbhsl0);
/*According to reference mannual, device mode setting has to be set by access usb host register */
*((uint32_t *)(USBFSH_BASE + 0x5C)) |= USBFSH_PORTMODE_DEV_ENABLE_MASK;
/* disable usb0 host clock */
CLOCK_DisableClock(kCLOCK_Usbhsl0);
USB_DeviceApplicationInit();
}

the output will be seen in the PC, that the mouse cursor will rotate in a square shape.

 

Thanking You,

Karthikeyan.

0 Kudos
Reply
3,215 Views
Karthikeyan_J
Contributor II

Hi,

 Zhangjennie

Thanks for your reply,

Demo code name and version of SDK are

name='SDK_2.x_LPCXpress54628'

version='2.8.2'

MCUXpresso IDE v11.2.0

Example program name:dev_hid_mouse_bm and freertos too.

this was the program which i cannot get the ouput that the moving cursor on the pc.

example program description is:

The USB HID mouse application is a simple demonstration program based on the MCUXpresso SDK.It is enumerated as a mouse. Users can see the mouse arrow moving on the PC screen according in a rectangular fashion.

Thanking You,

Karthikeyan J

0 Kudos
Reply