how configure keil for use from external sram as default heap location

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how configure keil for use from external sram as default heap location

1,585 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alireza sd on Sun Apr 27 00:23:07 MST 2014
Hi to all
I am beginner in embedded systems so I need your helps.
Recently I was working on a training project and on it I use from lpc1788 with 2mb * 16bit external ram,i successfully use from external memory as buffer of LCD controller, but i can not configure my compiler to use from it as default heap location(my compiler is keil v5),
Now any one can give me a guide that how can i configure keil for use from external memory as default heap location.
Excuse me for my bad English.
Thanks for your attention.
标签 (1)
0 项奖励
回复
1 回复

1,226 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri May 16 17:27:28 MST 2014
Defining __initial_sp, __heap_base and __heap_limit
Home » The ARM C and C++ libraries » Defining __initial_sp, __heap_base and __heap_limi
One of several methods you can use to specify the initial stack pointer and heap bounds is to define the following symbols:
•__initial_sp
•__heap_base
•__heap_limit.
You can define these symbols in an assembly language file, or by using the embedded assembler in C.
For example:
__asm void dummy_function(void)
{
    EXPORT __initial_sp
    EXPORT __heap_base
    EXPORT __heap_limit

__initial_sp EQU STACK_BASE
__heap_base EQU HEAP_BASE
__heap_limit EQU (HEAP_BASE + HEAP_SIZE)
}
The constants STACK_BASE, HEAP_BASE and HEAP_SIZE can be defined in a header file, for example stack.h, as follows:
/* stack.h */
#define HEAP_BASE 0x20100000  /* Example memory addresses */
#define STACK_BASE 0x20200000
#define HEAP_SIZE ((STACK_BASE-HEAP_BASE)/2)
#define STACK_SIZE ((STACK_BASE-HEAP_BASE)/2)
Note
This method of specifying the initial stack pointer and heap bounds is supported by both the standard C library (standardlib) and the micro C library (microlib).
0 项奖励
回复