how can I get source of libusbd_177x_8x_lib ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can I get source of libusbd_177x_8x_lib ?

981 Views
walm_nxp
Contributor II

I tried to create composite USB-Device with MSC and HID-Keyboard, but I always get 'ERR_USBD_BAD_EP_DESC' at call USBD_API->hid->init(). MSC is working normal. Also HID Keyboard is working normal if used stand-alone.

So I try to find reason of problem at debug libusbd_177x_8x_lib, but source-code is needed to do.

0 Kudos
Reply
1 Reply

864 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if this helps.

lpcopen v2.10 - USB on 17xx devices 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------



0 Kudos
Reply