help on J-link program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

help on J-link program

2,427 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zhangsr on Fri Oct 28 16:29:55 MST 2011
hi, what setup should i configure to use J-link to program the external nor flash?
Thanks
Labels (1)
0 Kudos
Reply
4 Replies

2,318 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RKRobinson on Thu Mar 27 07:08:01 MST 2014
Hi,
Here is a J-FLASH file that allows programming of external flash connected to an LPC1788. Obviously you must rename the file and remove the ".txt" extension.
Regards,
Richard.
0 Kudos
Reply

2,318 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by usb10185 on Thu Nov 03 13:41:29 MST 2011
You can use the LPC2478_EmbeddedArtists_1x16_CFI.jflash as a reference to get running with the LPC1788, see C:\Program Files (x86)\SEGGER\JLinkARM_V429a\Samples\JFlash\ProjectFiles

The LPC1768 does not have external flash.

0 Kudos
Reply

2,318 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zhangsr on Wed Nov 02 15:24:37 MST 2011
hi, we are using lpc1788.
we can only find lpc1768 project file but it doesn't work.

Thanks
0 Kudos
Reply

2,318 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by usb10185 on Sun Oct 30 15:04:37 MST 2011
What LPC part are you trying to program?
JLINK has a selection of configurations already available in the Segger install directory:
C:\Program Files (x86)\SEGGER\JLinkARM_V429a\Samples\JFlash\ProjectFiles
0 Kudos
Reply