gipo counter?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gipo counter?

1,308 Views
aravindpb5009
Contributor III

hai

     how to act one GPIO PIN as counter if any example is there . Iam using Lpc824 mcuxpresso 

Thanks & Regards

Aravind P

Labels (1)
0 Kudos
Reply
1 Reply

1,260 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Aravind palanisamy,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'm not very clear with your purpose, whether you want the GPIO to detect the number of the input pulse.
If yes, I'd like to suggest you refer to the pint_pin_interrupt demo in the  LPCXpresso824MAX's code bundle whose download link is below.
https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/general-p...

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply