gipo counter?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gipo counter?

1,313件の閲覧回数
aravindpb5009
Contributor III

hai

     how to act one GPIO PIN as counter if any example is there . Iam using Lpc824 mcuxpresso 

Thanks & Regards

Aravind P

ラベル(1)
0 件の賞賛
返信
1 返信

1,265件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Aravind palanisamy,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'm not very clear with your purpose, whether you want the GPIO to detect the number of the input pulse.
If yes, I'd like to suggest you refer to the pint_pin_interrupt demo in the  LPCXpresso824MAX's code bundle whose download link is below.
https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/general-p...

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信