fsl_power.c for LPC844 vs 845

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl_power.c for LPC844 vs 845

3,816件の閲覧回数
HeMyFAE
NXP Employee
NXP Employee

DEar LPC 804 SDK team,

It seems that two FSL_POWER.c from 844 SDK vs 845 SDK are different.

844's  fsl_power.c is much smaller and missing quite a few low power options compare to 845's.

Please advise!

hy

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,718件の閲覧回数
HeMyFAE
NXP Employee
NXP Employee

HI Jeremy,

I don't see what you're talking about.

I unzipped your zip package below.

if you can see, in the 844 directory, the fsl_power.c file is only 2k and in the 845 directory, the fsl_power.c file is 5k.

There is a big difference in the two files if you exam it closely.

Regards,

hy

pastedImage_1.png

pastedImage_2.png

3,718件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thanks for your reply, and I see it now.
I'll report this situation in the next round of field trials of the SDK library.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,718件の閲覧回数
HeMyFAE
NXP Employee
NXP Employee

Sorry I got my title mixed up.

It should be LPC844 and LPC845. The SDK are the latest 2.7.

Regards,

hy

0 件の賞賛
返信

3,718件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thanks for your reply.
After building an SDK library for the LPC844, I find this fsl_power.c is as same as the fsl_power.c that comes from the LPC845's SDK library.
I've attached the SDK library, please check it.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,718件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Before answering your question, I'd like to confirm something with you.
1) Is it LPC804 or LPC844?
2) Which revision of SDK library does the fsl_power.c come from?

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信