firmware update using a UART for the LPC21xx device and LPC1549 device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

firmware update using a UART for the LPC21xx device and LPC1549 device

3,030件の閲覧回数
andrewbarningha
Contributor III

Dear support,

Can you advise me if you do any packages where i can do a firmware update or download some firmware through the RS232 port on a linux system.

I have been using a product called flash magic but this doesn't seem to friendly with linux.

Any suggestions would be appreciated.

Thanks

Andrew

3 返答(返信)

2,862件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Andrew, 

You can try the utility that Con Verse is saying. Another option is to develop your own utility, you can use the next application note https://www.nxp.com/docs/en/application-note/AN11229.pdf  as a guide to see how you need to send the data through RS232. 

Regards,

Victor.

2,862件の閲覧回数
converse
Senior Contributor V

Lpcscrypt won't help you as it for LPC18/43 parts.

you might try this open source utility - mxil

mxli - Marc's exquisite LPC ISP tool 

2,862件の閲覧回数
andrewbarningha
Contributor III

Thanks

0 件の賞賛
返信