example code for usb virtual com port using lpc1768

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

example code for usb virtual com port using lpc1768

2,954件の閲覧回数
dpsodha
Contributor I

Dear sirs,

I need example code for usb virtual com port to communicate data to pc windows 7.

Thanks.

With regards

Dinesh

ラベル(1)
0 件の賞賛
返信
1 返信

2,735件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

I suggest to use the usbd_lib_composite LPCOpen example code. In this example and virtual comm port interface (using CDC-ACM class) and a HID-mouse interfaces are combined together to form a composite device. The VCOM interface
could be used for out putting debug messages.

You can download LPCOpen from the following link:

LPCOpen Software for LPC17XX | NXP 

Regards 

Sol 

0 件の賞賛
返信