ethernet on hitex 4350 eval board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ethernet on hitex 4350 eval board

1,294 Views
Icio
Contributor I

Hi,
I am trying to run sa_tcpecho-spifi_hitex_eva_4350 example on Hitex 4350 eval board. This is an example
with lwIP stack without an RTOS, provided by LPCOPEN. I selected MII interface.
I checked all jumper setting required for etehernet as described in "Quickstart_LPC1850EVA-LPC4350-A4.pdf".
I set a static IP address on the code.
When I plug in a ethernet cable the code realize the event, but when I make a ping to that IP address
I have no response.
The example doesn't work. Is there any specific setting that need to be done in the code or on the hitex
eval board to make the ethernet work?
thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,181 Views
soledad
NXP Employee
NXP Employee

Hi Maurizio,

Please check the below thread and let me know if this helps. 

LwIP sample fail 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply