ethernet on hitex 4350 eval board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ethernet on hitex 4350 eval board

1,296件の閲覧回数
Icio
Contributor I

Hi,
I am trying to run sa_tcpecho-spifi_hitex_eva_4350 example on Hitex 4350 eval board. This is an example
with lwIP stack without an RTOS, provided by LPCOPEN. I selected MII interface.
I checked all jumper setting required for etehernet as described in "Quickstart_LPC1850EVA-LPC4350-A4.pdf".
I set a static IP address on the code.
When I plug in a ethernet cable the code realize the event, but when I make a ping to that IP address
I have no response.
The example doesn't work. Is there any specific setting that need to be done in the code or on the hitex
eval board to make the ethernet work?
thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,183件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Maurizio,

Please check the below thread and let me know if this helps. 

LwIP sample fail 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信