enhanced boot mcuexpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

enhanced boot mcuexpresso

ソリューションへジャンプ
4,422件の閲覧回数
benmalchow
Contributor II

Is there any MCU_Expresso compatible assembly to do the following for the LPCXpresso54608?

3.3.2.6 Modifications to startup code to enable enhanced boot support
Several modifications need to be made to the startup code to enable enhanced boot
support. The value at offset 0x24 in the image must contain an enhanced image marker
and the value at offset 0x28 must point to a valid image header in the image. See the box
below for an example setup using a Single Enhanced image. Changes are in bold and
made to the vector table are of the startup code.
; Vector Table Mapped to Address 0 at Reset
AREA RESET, DATA, READONLY
EXPORT __Vectors
__Vectors DCD __initial_sp ; Top of Stack
DCD Reset_Handler ; Reset Handler
DCD NMI_Handler
DCD HardFault_Handler
DCD MemManage_Handler
DCD BusFault_Handler
DCD UsageFault_Handler
__vector_table_0x1c
DCD 0 ; Checksum of the first 7 words
DCD 0
DCD 0xEDDC9494 ; Enhanced image marker, set to 0x0 for legacy boot
IMPORT imageHeader
UM10912 All information provided in this document is subject to legal disclaimers. © NXP Semiconductors N.V. 2017. All rights reserved.
User manual Rev. 2.1 — 9 November 2017 30 of 1174
NXP Semiconductors UM10912
Chapter 3: LPC546xx Boot process
DCD imageHeader ; Pointer to enhanced image header, use 0x0 for legacy
boot
The image header for the startup code must be located somewhere in non-volatile
memory. A simple image header that doesn’t perform CRC is shown below. All field sizes
are 32-bits.
/* Image header */
const IMAGEHEADER_T imageHeader = {
IMAGE_ENH_BLOCK_MARKER, /* Required marker for image header */
IMG_NO_CRC, /* No CRC, makes development easier */
0x00000000, /* crc32_len */
0x00000000, /* crc32_val */
0x00000000 /* version */
};

I cannot get the IDE/assembler to recognize any of the arm instructions.

Thanks!

Ben

ラベル(1)
0 件の賞賛
返信
1 解決策
3,804件の閲覧回数
benmalchow
Contributor II

I resolved my issue.

I had section variables that were overwriting first 7 words starting at FLASH address 0x0.

Used Vector table in .C to enable single enhanced image:

__attribute__ ((used, section(".isr_vector")))
void (* const g_pfnVectors_Boot[])(void) = {
// Core Level - CM4
&_vStackTop, // The initial stack pointer
ResetISR, // The reset handler
NMI_Handler, // The NMI handler
HardFault_Handler, // The hard fault handler
MemManage_Handler, // The MPU fault handler
BusFault_Handler, // The bus fault handler
UsageFault_Handler, // The usage fault handler
__valid_user_code_checksum, // LPC MCU checksum
0, // ECRP
SINGLE_ENHANCED_IMAGE_SIGNATURE, // Reserved
(void *) &image_header, // Reserved
SVC_Handler, // SVCall handler
DebugMon_Handler, // Debug monitor handler
0, // Reserved
PendSV_Handler, // The PendSV handler
SysTick_Handler, // The SysTick handler

// Chip Level - LPC54608
WDT_BOD_IRQHandler, // 16: Windowed watchdog timer, Brownout detect
DMA0_IRQHandler, // 17: DMA controller
GINT0_IRQHandler, // 18: GPIO group 0
GINT1_IRQHandler, // 19: GPIO group 1
PIN_INT0_IRQHandler, // 20: Pin interrupt 0 or pattern match engine slice 0
PIN_INT1_IRQHandler, // 21: Pin interrupt 1or pattern match engine slice 1
PIN_INT2_IRQHandler, // 22: Pin interrupt 2 or pattern match engine slice 2
PIN_INT3_IRQHandler, // 23: Pin interrupt 3 or pattern match engine slice 3
UTICK0_IRQHandler, // 24: Micro-tick Timer
MRT0_IRQHandler, // 25: Multi-rate timer
CTIMER0_IRQHandler, // 26: Standard counter/timer CTIMER0
CTIMER1_IRQHandler, // 27: Standard counter/timer CTIMER1
SCT0_IRQHandler, // 28: SCTimer/PWM
CTIMER3_IRQHandler, // 29: Standard counter/timer CTIMER3
FLEXCOMM0_IRQHandler, // 30: Flexcomm Interface 0 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM1_IRQHandler, // 31: Flexcomm Interface 1 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM2_IRQHandler, // 32: Flexcomm Interface 2 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM3_IRQHandler, // 33: Flexcomm Interface 3 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM4_IRQHandler, // 34: Flexcomm Interface 4 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM5_IRQHandler, // 35: Flexcomm Interface 5 (USART, SPI, I2C,, FLEXCOMM)
FLEXCOMM6_IRQHandler, // 36: Flexcomm Interface 6 (USART, SPI, I2C, I2S,, FLEXCOMM)
FLEXCOMM7_IRQHandler, // 37: Flexcomm Interface 7 (USART, SPI, I2C, I2S,, FLEXCOMM)
ADC0_SEQA_IRQHandler, // 38: ADC0 sequence A completion.
ADC0_SEQB_IRQHandler, // 39: ADC0 sequence B completion.
ADC0_THCMP_IRQHandler, // 40: ADC0 threshold compare and error.
DMIC0_IRQHandler, // 41: Digital microphone and DMIC subsystem
HWVAD0_IRQHandler, // 42: Hardware Voice Activity Detector
USB0_NEEDCLK_IRQHandler, // 43: USB Activity Wake-up Interrupt
USB0_IRQHandler, // 44: USB device
RTC_IRQHandler, // 45: RTC alarm and wake-up interrupts
Reserved46_IRQHandler, // 46: Reserved interrupt
Reserved47_IRQHandler, // 47: Reserved interrupt
PIN_INT4_IRQHandler, // 48: Pin interrupt 4 or pattern match engine slice 4 int
PIN_INT5_IRQHandler, // 49: Pin interrupt 5 or pattern match engine slice 5 int
PIN_INT6_IRQHandler, // 50: Pin interrupt 6 or pattern match engine slice 6 int
PIN_INT7_IRQHandler, // 51: Pin interrupt 7 or pattern match engine slice 7 int
CTIMER2_IRQHandler, // 52: Standard counter/timer CTIMER2
CTIMER4_IRQHandler, // 53: Standard counter/timer CTIMER4
RIT_IRQHandler, // 54: Repetitive Interrupt Timer
SPIFI0_IRQHandler, // 55: SPI flash interface
FLEXCOMM8_IRQHandler, // 56: Flexcomm Interface 8 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM9_IRQHandler, // 57: Flexcomm Interface 9 (USART, SPI, I2C, FLEXCOMM)
SDIO_IRQHandler, // 58: SD/MMC
CAN0_IRQ0_IRQHandler, // 59: CAN0 interrupt0
CAN0_IRQ1_IRQHandler, // 60: CAN0 interrupt1
CAN1_IRQ0_IRQHandler, // 61: CAN1 interrupt0
CAN1_IRQ1_IRQHandler, // 62: CAN1 interrupt1
USB1_IRQHandler, // 63: USB1 interrupt
USB1_NEEDCLK_IRQHandler, // 64: USB1 activity
ETHERNET_IRQHandler, // 65: Ethernet
ETHERNET_PMT_IRQHandler, // 66: Ethernet power management interrupt
ETHERNET_MACLP_IRQHandler, // 67: Ethernet MAC interrupt
EEPROM_IRQHandler, // 68: EEPROM interrupt
LCD_IRQHandler, // 69: LCD interrupt
SHA_IRQHandler, // 70: SHA interrupt
SMARTCARD0_IRQHandler, // 71: Smart card 0 interrupt
SMARTCARD1_IRQHandler, // 72: Smart card 1 interrupt
}; /* End of g_pfnVectors */

...  Poor understanding on my part.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,804件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the LPC1700 secondary USB bootloader as reference:

 

http://cache.nxp.com/docs/en/application-note/AN10866.zip

 

I hope this helps,

Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,804件の閲覧回数
benmalchow
Contributor II

I have gotten past one of my hurdles.  I have a section placement variable to write the single enhanced image enable to 0x24 in FLASH.  At 0x28 I have the pointer to the image header which I stored in .rodata.

The ROM bootloader successfully jumps to my single enhanced image (this will be my secondary bootloader).  My secondary bootloader consumes FLASH space 0x0 to 0x7FFF.  I created a dummy app that blinks LEDS, it consumes FLASH space 0x8000 to 0x7FFFF.  My secondary bootloader, at this moment, simply jumps to my dummy app.

When I flash the dummy app, then flash the secondary bootlaoder all works well (I see blinking LEDS).

However, when I reset I end up in some invalid memory space:

invalid_mem.jpg

Any thoughts would be greatly appreciated!

PS, I have loaded additional symbol files in the bootloader so I can debug both bootloader and application, so this is likely not a debug issue.

Thanks!

Ben

0 件の賞賛
返信
3,805件の閲覧回数
benmalchow
Contributor II

I resolved my issue.

I had section variables that were overwriting first 7 words starting at FLASH address 0x0.

Used Vector table in .C to enable single enhanced image:

__attribute__ ((used, section(".isr_vector")))
void (* const g_pfnVectors_Boot[])(void) = {
// Core Level - CM4
&_vStackTop, // The initial stack pointer
ResetISR, // The reset handler
NMI_Handler, // The NMI handler
HardFault_Handler, // The hard fault handler
MemManage_Handler, // The MPU fault handler
BusFault_Handler, // The bus fault handler
UsageFault_Handler, // The usage fault handler
__valid_user_code_checksum, // LPC MCU checksum
0, // ECRP
SINGLE_ENHANCED_IMAGE_SIGNATURE, // Reserved
(void *) &image_header, // Reserved
SVC_Handler, // SVCall handler
DebugMon_Handler, // Debug monitor handler
0, // Reserved
PendSV_Handler, // The PendSV handler
SysTick_Handler, // The SysTick handler

// Chip Level - LPC54608
WDT_BOD_IRQHandler, // 16: Windowed watchdog timer, Brownout detect
DMA0_IRQHandler, // 17: DMA controller
GINT0_IRQHandler, // 18: GPIO group 0
GINT1_IRQHandler, // 19: GPIO group 1
PIN_INT0_IRQHandler, // 20: Pin interrupt 0 or pattern match engine slice 0
PIN_INT1_IRQHandler, // 21: Pin interrupt 1or pattern match engine slice 1
PIN_INT2_IRQHandler, // 22: Pin interrupt 2 or pattern match engine slice 2
PIN_INT3_IRQHandler, // 23: Pin interrupt 3 or pattern match engine slice 3
UTICK0_IRQHandler, // 24: Micro-tick Timer
MRT0_IRQHandler, // 25: Multi-rate timer
CTIMER0_IRQHandler, // 26: Standard counter/timer CTIMER0
CTIMER1_IRQHandler, // 27: Standard counter/timer CTIMER1
SCT0_IRQHandler, // 28: SCTimer/PWM
CTIMER3_IRQHandler, // 29: Standard counter/timer CTIMER3
FLEXCOMM0_IRQHandler, // 30: Flexcomm Interface 0 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM1_IRQHandler, // 31: Flexcomm Interface 1 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM2_IRQHandler, // 32: Flexcomm Interface 2 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM3_IRQHandler, // 33: Flexcomm Interface 3 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM4_IRQHandler, // 34: Flexcomm Interface 4 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM5_IRQHandler, // 35: Flexcomm Interface 5 (USART, SPI, I2C,, FLEXCOMM)
FLEXCOMM6_IRQHandler, // 36: Flexcomm Interface 6 (USART, SPI, I2C, I2S,, FLEXCOMM)
FLEXCOMM7_IRQHandler, // 37: Flexcomm Interface 7 (USART, SPI, I2C, I2S,, FLEXCOMM)
ADC0_SEQA_IRQHandler, // 38: ADC0 sequence A completion.
ADC0_SEQB_IRQHandler, // 39: ADC0 sequence B completion.
ADC0_THCMP_IRQHandler, // 40: ADC0 threshold compare and error.
DMIC0_IRQHandler, // 41: Digital microphone and DMIC subsystem
HWVAD0_IRQHandler, // 42: Hardware Voice Activity Detector
USB0_NEEDCLK_IRQHandler, // 43: USB Activity Wake-up Interrupt
USB0_IRQHandler, // 44: USB device
RTC_IRQHandler, // 45: RTC alarm and wake-up interrupts
Reserved46_IRQHandler, // 46: Reserved interrupt
Reserved47_IRQHandler, // 47: Reserved interrupt
PIN_INT4_IRQHandler, // 48: Pin interrupt 4 or pattern match engine slice 4 int
PIN_INT5_IRQHandler, // 49: Pin interrupt 5 or pattern match engine slice 5 int
PIN_INT6_IRQHandler, // 50: Pin interrupt 6 or pattern match engine slice 6 int
PIN_INT7_IRQHandler, // 51: Pin interrupt 7 or pattern match engine slice 7 int
CTIMER2_IRQHandler, // 52: Standard counter/timer CTIMER2
CTIMER4_IRQHandler, // 53: Standard counter/timer CTIMER4
RIT_IRQHandler, // 54: Repetitive Interrupt Timer
SPIFI0_IRQHandler, // 55: SPI flash interface
FLEXCOMM8_IRQHandler, // 56: Flexcomm Interface 8 (USART, SPI, I2C, FLEXCOMM)
FLEXCOMM9_IRQHandler, // 57: Flexcomm Interface 9 (USART, SPI, I2C, FLEXCOMM)
SDIO_IRQHandler, // 58: SD/MMC
CAN0_IRQ0_IRQHandler, // 59: CAN0 interrupt0
CAN0_IRQ1_IRQHandler, // 60: CAN0 interrupt1
CAN1_IRQ0_IRQHandler, // 61: CAN1 interrupt0
CAN1_IRQ1_IRQHandler, // 62: CAN1 interrupt1
USB1_IRQHandler, // 63: USB1 interrupt
USB1_NEEDCLK_IRQHandler, // 64: USB1 activity
ETHERNET_IRQHandler, // 65: Ethernet
ETHERNET_PMT_IRQHandler, // 66: Ethernet power management interrupt
ETHERNET_MACLP_IRQHandler, // 67: Ethernet MAC interrupt
EEPROM_IRQHandler, // 68: EEPROM interrupt
LCD_IRQHandler, // 69: LCD interrupt
SHA_IRQHandler, // 70: SHA interrupt
SMARTCARD0_IRQHandler, // 71: Smart card 0 interrupt
SMARTCARD1_IRQHandler, // 72: Smart card 1 interrupt
}; /* End of g_pfnVectors */

...  Poor understanding on my part.

0 件の賞賛
返信
3,804件の閲覧回数
converse
Senior Contributor V

What errors are you getting? Perhaps post the code you are trying to assemble?

0 件の賞賛
返信
3,804件の閲覧回数
benmalchow
Contributor II

After further digging it's due to the toolchain used by MCUXpresso.  I either need the assembly for ARM-GCC to accomplish this, or the equivalent code in C.

I will try to port in the meantime.

Thanks!

Ben

0 件の賞賛
返信