enabling the LPC1768FET100 ISP command handler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

enabling the LPC1768FET100 ISP command handler

3,391 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by digysol on Mon Feb 02 11:43:04 MST 2015
Looking for sample code to start the ISP command handler. C code that just shows how the initialization sequence for the RESET pin and the P2.10 pin are handled to enable the ISP command handler will be ideal.
Labels (1)
0 Kudos
Reply
8 Replies

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by digysol on Thu Feb 05 13:29:18 MST 2015
R2D2,

Thank you and may the force be with you :-)
0 Kudos
Reply

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Feb 04 14:17:04 MST 2015

Quote: digysol
The code sample in 'Reinvoke ISP' involves user coxde running within the LPC17xx flash, as I understand.

What I am looking for is remote start of the bootloader in the LPC17xx from another processor.



If you don't want to implement "Reinvoke ISP' (and use it together with reading an input pin) then just add transistors to P2.10 and Reset. Then pull P2.10 low and after that pull Reset low a few ms, just like switching to ISP with buttons...
0 Kudos
Reply

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by digysol on Wed Feb 04 13:57:26 MST 2015
The code sample in 'Reinvoke ISP' involves user coxde running within the LPC17xx flash, as I understand.

What I am looking for is remote start of the bootloader in the LPC17xx from another processor.
0 Kudos
Reply

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Feb 03 13:24:09 MST 2015

Quote: digysol
Start the bootloader.



So what's wrong with 'Reinvoke ISP'  :quest:
0 Kudos
Reply

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by digysol on Tue Feb 03 13:18:07 MST 2015
Start the bootloader.
0 Kudos
Reply

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Feb 02 13:29:17 MST 2015

Quote: digysol
Just to clarify, I need sample code related to section 32.3 of the LPC176x/5x user manual (page 624).



:quest:  :quest:

To do what?  Start the bootloader? Program the flash? Rule the world?
0 Kudos
Reply

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by digysol on Mon Feb 02 13:23:02 MST 2015
Just to clarify, I need sample code related to section 32.3 of the LPC176x/5x user manual (page 624).
0 Kudos
Reply

3,323 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Feb 02 12:10:29 MST 2015
:quest:

Are we talking about 'Reinvoke ISP' (IAP57)  :quest:
0 Kudos
Reply