emWin widget listwheel doesn't work correctly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emWin widget listwheel doesn't work correctly

1,708 Views
hkroeger
Contributor I

Hello,

I'm using emWin with freertos. emWin works fine, but after a few hours oder days i can't change values with the listwheel widget. The wheel doesn't turn anymore. All Buttons and Sliders works. After a hard reset everything works fine.

Could it a problem from emWin or a combiniton with freertos?

I'm using the LPC4357JET256.

0 Kudos
Reply
1 Reply

1,324 Views
soledad
NXP Employee
NXP Employee

Hi,

I redirected this issue to SEGGER forum. Please check the following thread

emWin widget listwheel doesn't work correctly - emWin related - SEGGER Forum 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply