emWin: prevent LISTBOX getting input focus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin: prevent LISTBOX getting input focus

2,613件の閲覧回数
ekki
Contributor III

Dear ladies and gentlemen,

in emWin:

How do I prevent a LISTBOX-widget from getting the input focus ?

The BUTTON-widget or the EDIT-widget have the <Widget>_SetFocussed() function. But LISTBOX doesn't. Is there another possibility?

Thanks in advance for any hint.

Regards,

Ekki 

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,104件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

 

I redirected this issue to SEGGER forum. Please check the following thread

emWin: prevent LISTBOX getting input focus - emWin related - SEGGER Forum 

 


Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,104件の閲覧回数
ekki
Contributor III

@ Sol:

Thanks, for your help. The hint I got there was perfect.

Best Regards,

Ekki

0 件の賞賛
返信