emWin: prevent LISTBOX getting input focus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emWin: prevent LISTBOX getting input focus

2,676 Views
ekki
Contributor III

Dear ladies and gentlemen,

in emWin:

How do I prevent a LISTBOX-widget from getting the input focus ?

The BUTTON-widget or the EDIT-widget have the <Widget>_SetFocussed() function. But LISTBOX doesn't. Is there another possibility?

Thanks in advance for any hint.

Regards,

Ekki 

Labels (2)
0 Kudos
Reply
2 Replies

2,167 Views
soledad
NXP Employee
NXP Employee

Hi,

 

I redirected this issue to SEGGER forum. Please check the following thread

emWin: prevent LISTBOX getting input focus - emWin related - SEGGER Forum 

 


Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,167 Views
ekki
Contributor III

@ Sol:

Thanks, for your help. The hint I got there was perfect.

Best Regards,

Ekki

0 Kudos
Reply