emWin on MCB4357 - Can't make it work...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin on MCB4357 - Can't make it work...

2,287件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DT1 on Wed Nov 06 10:45:42 MST 2013
Hi,

Anybody managed to make emWin work on a Keil MCB4357 v1.3?

As a base, I'm using the downloaded LPCWare example named "LPC4357-EVB emWin". It uses the Lin driver and uses the SDRAM for memory. That example seems to be for another board (the Hitex one?), so I changed pin attribution for the Backlight.

Upon calling GUI_Init(), my backlight is ON, but I can't put anything on the screen...

Some functions :

{
...
        if (GUI_Init() != 0)
{
goto END;
}

// Do some drawing tests.
GUI_SetBkColor(GUI_RED);
GUI_Clear();
GUI_Delay(1000);
GUI_SetBkColor(GUI_GREEN);
GUI_Clear();
GUI_Delay(1000);
GUI_SetBkColor(GUI_BLUE);
GUI_Clear();
GUI_Delay(1000);

GUI_SetBkColor(GUI_BLACK);
GUI_Clear();
...
}




void LCD_X_Init(void)
{
int  i;

// Configure the operating mode for involved pins.
  scu_pinmux(NBSP_MCUPIN_LCD_DOTCLK_PORT,NBSP_MCUPIN_LCD_DOTCLK_PIN, MD_PUP, NBSP_MCUPIN_LCD_DOTCLK_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VSYNC_PORT, NBSP_MCUPIN_LCD_VSYNC_PIN, MD_PUP, NBSP_MCUPIN_LCD_VSYNC_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_ENABLE_PORT, NBSP_MCUPIN_LCD_ENABLE_PIN, MD_PUP, NBSP_MCUPIN_LCD_ENABLE_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_HSYNC_PORT, NBSP_MCUPIN_LCD_HSYNC_PIN, MD_PUP, NBSP_MCUPIN_LCD_HSYNC_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_BL_EN_PORT, NBSP_MCUPIN_LCD_BL_EN_PIN, MD_PUP, NBSP_MCUPIN_LCD_BL_EN_PIN_MODE);// Used as GPIO.

scu_pinmux(NBSP_MCUPIN_LCD_VD0_PORT, NBSP_MCUPIN_LCD_VD0_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD0_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD1_PORT, NBSP_MCUPIN_LCD_VD1_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD1_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD2_PORT, NBSP_MCUPIN_LCD_VD2_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD2_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD3_PORT, NBSP_MCUPIN_LCD_VD3_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD3_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD4_PORT, NBSP_MCUPIN_LCD_VD4_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD4_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD5_PORT, NBSP_MCUPIN_LCD_VD5_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD5_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD6_PORT, NBSP_MCUPIN_LCD_VD6_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD6_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD7_PORT, NBSP_MCUPIN_LCD_VD7_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD7_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD8_PORT, NBSP_MCUPIN_LCD_VD8_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD8_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD9_PORT, NBSP_MCUPIN_LCD_VD9_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD9_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD10_PORT, NBSP_MCUPIN_LCD_VD10_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD10_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD11_PORT, NBSP_MCUPIN_LCD_VD11_PIN,MD_PUP, NBSP_MCUPIN_LCD_VD11_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD12_PORT, NBSP_MCUPIN_LCD_VD12_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD12_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD13_PORT, NBSP_MCUPIN_LCD_VD13_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD13_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD14_PORT, NBSP_MCUPIN_LCD_VD14_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD14_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD15_PORT, NBSP_MCUPIN_LCD_VD15_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD15_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD16_PORT, NBSP_MCUPIN_LCD_VD16_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD16_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD17_PORT, NBSP_MCUPIN_LCD_VD17_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD17_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD18_PORT, NBSP_MCUPIN_LCD_VD18_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD18_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD19_PORT, NBSP_MCUPIN_LCD_VD19_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD19_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD20_PORT, NBSP_MCUPIN_LCD_VD20_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD20_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD21_PORT, NBSP_MCUPIN_LCD_VD21_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD21_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD22_PORT, NBSP_MCUPIN_LCD_VD22_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD22_PIN_MODE);
scu_pinmux(NBSP_MCUPIN_LCD_VD23_PORT, NBSP_MCUPIN_LCD_VD23_PIN, MD_PUP, NBSP_MCUPIN_LCD_VD23_PIN_MODE);

// Set direction for GPIO pins.
GPIO_SetDir(NBSP_DO_LCD_BL_EN_GPIO_PORT, GPIO_PIN_MASK(NBSP_DO_LCD_BL_EN_GPIO_PIN), NBSP_GPIO_DIR_OUTPUT);

// Delay.
for(i = 0; i < 1000000; i++);

LPC_RGU->RESET_CTRL0 = (1U << 16);
while ((LPC_RGU->RESET_ACTIVE_STATUS0 & (1U << 16)) == 0);

LPC_LCD->CTRL &= ~(1 << 0);           /* Disable LCD                        */
LPC_LCD->INTMSK = 0;                  /* Disable all interrupts             */
 
LCD_Init_CFG(LPC_LCD, (LCD_CFG_Type*)&Sharp);
LCD_SetFrameBuffer(LPC_LCD, (void*)0x28000000);
LCD_Power(LPC_LCD, ENABLE);

// Delay.
for(i = 0; i < 1000000; i++);

// Enable Backlight
GPIO_SetValue(NBSP_DO_LCD_BL_EN_GPIO_PORT, GPIO_PIN_MASK(NBSP_DO_LCD_BL_EN_GPIO_PIN));
}
ラベル(1)
0 件の賞賛
返信
1 返信

2,183件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DT1 on Wed Nov 06 15:09:04 MST 2013
Ok, managed to get code from Keil of their MCB4357 and was missing the SPI part for init. Now it's working.
0 件の賞賛
返信