emWin libraries for uEZ V1.12 & Rowley  CW 2.1 compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emWin libraries for uEZ V1.12 & Rowley  CW 2.1 compiler

1,873 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jjreynolds2004 on Tue Dec 06 10:35:02 MST 2011
Hi,we have an FDI DK-TS-1788 kit running with uEZ V1.12b software. The uEZ software comes with emWin library header files and an option to run an emWin demo, but it does not have the *.a static
library files needed to link in the emWin demo. I see that SEGGER provides emWin demos to run on LPC1788 boards for KEIL and IAR compilers, but not for Rowley. Are there any *.a static emWin library files compatible with the Rowley compiler available ?

Thanks,
John Reynods
Labels (1)
0 Kudos
Reply
4 Replies

1,821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rfequip on Sat Sep 15 00:18:22 MST 2012
sorry for the duplicate post Window 7 is too slow
0 Kudos
Reply

1,821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rfequip on Sat Sep 15 00:16:03 MST 2012
Has any one been able to get the emWIN libraries working on the UEZ LPC1788 board with the 4.3" display working?  I am having a rough time.  I am using Crossworks 
0 Kudos
Reply

1,821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rfequip on Sat Sep 15 00:15:58 MST 2012
Has any one been able to get the emWIN libraries working on the UEZ LPC1788 board with the 4.3" display working?  I am having a rough time.  I am using Crossworks 
0 Kudos
Reply

1,821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Wed Dec 07 03:17:00 MST 2011
There is currently no library for Crossworks for ARM (they are available exclusively for IAR, Keil and LPCXpresso).  While Crossworks support is planned there is currently no specific date for this, but it will be posted here when available.
0 Kudos
Reply