I am using the NXP emWin (5.38a) library running on an LPC1768 to drive a 800 x 480 pixel LCD panel using a Solomon SSD1963 controller. Starting with the MCB1700 bsp as a template, I have configured emWin to use the FlexColor driver with 16 bpp, no cache, and a 16 bit parallel bus, and allocated 30K bytes of RAM for emWin. The display initializes properly, and I can execute various graphical commands such as GUI_SetColor, GUI_FillCircle, GUI_Clear, GUI_SetBkColor, GUI_SetPenSize, GUI_Drawline, etc. However, if I try to display any text, such as GUI_DispString, I get a hard fault within the library function GUIMONO_DispChar(). Looking at the faults register I see:
Faults = UndefInstr
Fault PC = 0x00003D40
= GUIMONO_DispChar + 108 in section .text
= No line number information available for address 0x3d40 <GUIMONO_DispChar+108>
Fault status registers:
IPSR = 0x1000003: 3 (HardFault)
CFSR = 00010000 (Configurable Fault Status Register)
HFSR = 40000000 (Hard Fault Status Register)
DFSR = 00000000 (Debug Fault Status Register)
MMAR = e000edf8 [INVALID] (MemManage Fault Address Register)
BFAR = e000edf8 [INVALID] (Bus Fault Address Register)
AFSR = 00000000 (Auxiliary Fault Status Register)
I am at a loss as to why this is happening. Any clues as to what might be the cause of the problem?