emWin Simulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emWin Simulation

1,818 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rnuss on Thu Mar 01 10:38:52 MST 2012
Is the simulation feature included in the emWin download?  I don't see the simulation folder or any Microsoft Visual C++ files, as indicated in the emWin manual.
Labels (1)
0 Kudos
Reply
3 Replies

1,707 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kpax on Wed Apr 25 10:08:11 MST 2012
Hello ktownsend,

can you pls post the link that contains the solution files for visual studio 2008, cause the latest version has the files for VS2010 which unfortunately i do not have.

Thanks
Kpax
0 Kudos
Reply

1,707 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Sun Mar 11 18:47:48 MST 2012
The latest emWin package available here includes support for all three LCDs from Embedded Artists (3.2", 4.3" and 7"), as well as full support for the simulator using Visual Studio 2008 or Visual Studio 2010.  The package is currently limited to supporting Keil and Crossworks for ARM (more IDEs will be added), but for simulation purposes this should be fine as a starting point.
0 Kudos
Reply

1,707 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dill on Thu Mar 08 04:34:46 MST 2012
The emWin demo for my devboards (IAR 1788 SK) runs the emWin sim.
0 Kudos
Reply