emWin Simulation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

emWin Simulation

1,847 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rnuss on Thu Mar 01 10:38:52 MST 2012
Is the simulation feature included in the emWin download?  I don't see the simulation folder or any Microsoft Visual C++ files, as indicated in the emWin manual.
标签 (1)
0 项奖励
回复
3 回复数

1,736 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kpax on Wed Apr 25 10:08:11 MST 2012
Hello ktownsend,

can you pls post the link that contains the solution files for visual studio 2008, cause the latest version has the files for VS2010 which unfortunately i do not have.

Thanks
Kpax
0 项奖励
回复

1,736 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Sun Mar 11 18:47:48 MST 2012
The latest emWin package available here includes support for all three LCDs from Embedded Artists (3.2", 4.3" and 7"), as well as full support for the simulator using Visual Studio 2008 or Visual Studio 2010.  The package is currently limited to supporting Keil and Crossworks for ARM (more IDEs will be added), but for simulation purposes this should be fine as a starting point.
0 项奖励
回复

1,736 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dill on Thu Mar 08 04:34:46 MST 2012
The emWin demo for my devboards (IAR 1788 SK) runs the emWin sim.
0 项奖励
回复