emWin 5.38 Libraries for NXP Cortex M3 are not for Cortex M3!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin 5.38 Libraries for NXP Cortex M3 are not for Cortex M3!

ソリューションへジャンプ
6,233件の閲覧回数
MarcoAEE
Contributor II

If you try to compile with these libraries, many error like the following will be reported:

Error: L6366E: GUIAA_Char2.o attributes are not compatible with the provided cpu and fpu attributes .
Object GUIAA_Char2.o contains Build Attributes that are incompatible with the CPU attributes.
Tag_CPU_arch = ARM v7E-M (=13)

This happens because the library compilation target is a Cortex M4.

In the old emWin library packages there were different compilations for the different cortex architectures used by NXP.

The following link is in the emWin section of the NXP website:

Segger emWin 5.38 Libraries and Utilities for NXP Cortex M3/M4 MCUs

Is it possible to include at least the compilation for Cortex M3 and M4 as declared?

Thank you

ラベル(6)
0 件の賞賛
返信
1 解決策
5,516件の閲覧回数
ckphua
NXP Employee
NXP Employee

Here's the updated emWin library (ver 5.38b) with M3 included

emWin Graphics Library|NXP 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,516件の閲覧回数
hfuhruhurr
Contributor III

Hi,

any chance that there will be an updated emWin library for the LPC1700 MCUs?

Regards,

Rainer

0 件の賞賛
返信
5,516件の閲覧回数
hfuhruhurr
Contributor III

Would somebody at NXP please have the kindness to respond to this request?

I think, it's quite an important issue.

Thanks!

0 件の賞賛
返信
5,516件の閲覧回数
ckphua
NXP Employee
NXP Employee

It did not have the M3 library. We are in the process of updating the posting to include the M3 library.

Sorry for the error

0 件の賞賛
返信
5,517件の閲覧回数
ckphua
NXP Employee
NXP Employee

Here's the updated emWin library (ver 5.38b) with M3 included

emWin Graphics Library|NXP 

0 件の賞賛
返信