emWin 5.38 Libraries for NXP Cortex M3 are not for Cortex M3!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

emWin 5.38 Libraries for NXP Cortex M3 are not for Cortex M3!

跳至解决方案
6,135 次查看
MarcoAEE
Contributor II

If you try to compile with these libraries, many error like the following will be reported:

Error: L6366E: GUIAA_Char2.o attributes are not compatible with the provided cpu and fpu attributes .
Object GUIAA_Char2.o contains Build Attributes that are incompatible with the CPU attributes.
Tag_CPU_arch = ARM v7E-M (=13)

This happens because the library compilation target is a Cortex M4.

In the old emWin library packages there were different compilations for the different cortex architectures used by NXP.

The following link is in the emWin section of the NXP website:

Segger emWin 5.38 Libraries and Utilities for NXP Cortex M3/M4 MCUs

Is it possible to include at least the compilation for Cortex M3 and M4 as declared?

Thank you

0 项奖励
回复
1 解答
5,418 次查看
ckphua
NXP Employee
NXP Employee

Here's the updated emWin library (ver 5.38b) with M3 included

emWin Graphics Library|NXP 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
5,418 次查看
hfuhruhurr
Contributor III

Hi,

any chance that there will be an updated emWin library for the LPC1700 MCUs?

Regards,

Rainer

0 项奖励
回复
5,418 次查看
hfuhruhurr
Contributor III

Would somebody at NXP please have the kindness to respond to this request?

I think, it's quite an important issue.

Thanks!

0 项奖励
回复
5,418 次查看
ckphua
NXP Employee
NXP Employee

It did not have the M3 library. We are in the process of updating the posting to include the M3 library.

Sorry for the error

0 项奖励
回复
5,419 次查看
ckphua
NXP Employee
NXP Employee

Here's the updated emWin library (ver 5.38b) with M3 included

emWin Graphics Library|NXP 

0 项奖励
回复